This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
PGA309评估板,传感器信号:1.1mV/V, 阻抗:1K
一、设置电压输出0.5V-4.5V ,输出信号很稳定,线性非常好;
当设置为XTR117+PGA309 电流输出时,VEXC供电只能选择2.13V,然后换掉PGA309和XTR117之间的电阻为10K+3K,另外一个补偿电流的电阻为2.5M,然后用PGA309EVM标定之后可以4-20mA,但是跳动特别大,最大在几百个uA;麻烦问一下这个可能是什么地方引起的啊?
二、假如传感器信号:1.1mV/V,阻抗0.7K,这个需要怎么设置才能出来4-20mA啊?
楼主您好!
1,首先,PGA309做4-20mA没问题的,能够满足您的应用;
“当设置为XTR117+PGA309 电流输出时,VEXC供电只能选择2.13V,然后换掉PGA309和XTR117之间的电阻为10K+3K,另外一个补偿电流的电阻为2.5M,然后用PGA309EVM标定之后可以4-20mA,但是跳动特别大,最大���几百个uA;麻烦问一下这个可能是什么地方引起的啊?”
2,请问,VEXC只能选择2.13V是什么意思?
3,为什么要换掉PGA309和XTR117直接的电阻10K+3K,评估板上有10K,但是3K是在哪里看到的?
二、假如传感器信号:1.1mV/V,阻抗0.7K,这个需要怎么设置才能出来4-20mA啊?
4,用评估板做4-20mA输出,评估板不需要做任何改动,正确连接硬件,按照软件提示,校准就好了。
1.感谢您的解答:是这样的,我们现在的传感器阻抗是0.7K和1k的,灵敏度都是1.1mV/V的
第一次试验的时候是按电压测试的,接的传感器阻抗是0.7K的,用的评估板,电压输出设置为0.5V-4.5V,VEXC设置为3.4V ,校正完成之后,输出特别好;
然后我又设置成电流4-20mA输出,传感器阻抗还是接的0.7K的,VEXC还是设置为3.4V,校正完成之后电流输出最小可以到6mA左右,到不了4mA,后来查了PGA309和XTR117的资料,感觉可能是下面的原因:传感器阻抗太小0.7K,供电VEXC3.4V ,这个地方的电流=3.4/0,7k=4.8mA左右,所以导致最后的输出电流调整不到4mA,然后将VEXC设置1.3V,此时可以调整出最小电流4mA,但是满量程达不到16mA了,计算了一下传感器满量程输出为1.3*1.1mV=1.43mV,假如按最大放大倍数计算的话1.43*1152=1.647V,此时计算电流的最大输出1.647V/21.3K*100=7.73mA,显然到不了16mA,所以需要改变10+11.3K的电阻,但是然后用PGA309 Calculator 计算时发现,假如PGA Zero Scale Output设置为小于0.44V时,后面仿真出来的Voa3是不符合要求的,所以只能设置为大于0.44V;而XTR117前面的电阻值的必须不大于1.647/168*100=10.3K,而此时的最小电流为0.44V/10.3K*100=4.27mA,也就是说只能4.27mA-20.27mA了;
2,因为上面的计算,所以后面改为传感器的阻抗为1K,灵敏度仍然为1.1mV/V,然后进行校准,设置VEXC为3.4V时,发现最小电流仍然校准不到4mA,所以只能选择VEXC为2.13V来进行下面的试验,此时传感器的输出为2.13*1.1mV=2.343mV,最大的放大倍数可以到2.699V,所以如果想输出4-20mA,只能选择改变10+11.3K的电阻了,所以后来计算改成了10+3K的电阻了,然后另外一个191K的电阻改成2.5M的了,但是此时输出的电流特别的不稳定,一直在跳动,零点输出最小3.97mA,最大可以达到4.13mA.
上面就是我测试的过程,找了半天原因不知道哪个环节出了问题,帮帮忙,多谢啊