1、ICC+符合规格满足20~25mA,ICC-不符合规格,大约在-16mA左右;
2、IiH参数施加2V测试为38uA左右不符合规格,施加5V测试为150uA符合规格,请确认是否是资料编写错误。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ICC+符合规格满足20~25mA,ICC-不符合规格,大约在-16mA左右;
您好,供电电压是多大?如何测试的?
IiH参数施加2V测试为38uA左右不符合规格,施加5V测试为150uA符合规格,请确认是否是资料编写错误。
资料编写没有错误,您是如何测试的?
ICC参数-供电电压是±5V,测试逻辑是V+施加5V,V-施加-5V,EN管脚施加0V,测试V+、V-的电流,其余管脚悬空;
您这边验证下,将LMH6572搭建成单位跟随,输入电压为1/2Vs(双电源供电,输入即为0V),输出不接负载,悬空,再验证下流经VCC+ 和VCC-的电流大小。
Iih参数--供电电压是±5V,测试逻辑是V+施加5V,V-施加-5V,EN、SEL管脚分别施加2V电压测试对应电流,其余管脚悬空;
Iih的参数应该是没有错,我参考了之前的几个版本都是2V。
方便换一块IC再验证看下吗?
1、麻烦详细描述下单位跟随模式各管脚的状态,避免我理解有误差;
LMH 6572是一款专门用于视频信号的,内部增益固定=2的2选1开关器件,所以不像普通的运放,我们可以直接搭建为电压跟随,双电源供电的话参考电压直接为GND,单电源供电为1/2VCC,输出悬空测试即可,所以LMH6572的ICC测试我再看下。
IiH我使用了89FH、61RA两个批次共20只产品都是这个情况,您那边是否方便使用IC验证下,或者寄给我两只合格的IC样片。
好的,我这边去确认下,您是在TI官网购买的吗?