This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2828: 正常运行时,板卡温度达到了60℃,请问如何在设计电路前正确评估好发热呢?

Part Number: OPA2828

您好:

我们使用了opa2828双运放搭建了一个反相器和模拟滤波器。

在30mm*80mm的布板面积下,有且只有16个opa2828运放(正面8个反面8个),电源都是外面提供的。板卡为六层板,两层完整的地。

供电为+8V/-6V。

实际测试发现,静态条件下,板卡上的温度已经达到了60℃(室温20℃测得),可能会影响周围的温度敏感的传感器。

希望改版解决这个温度太高的问题。

因此,想请教下TI专家:

1、如何在电路设计前就评估好电路板的温度呢?我知道用芯片的热阻,和功率相乘可以得到芯片温升,加上环境温度判断是否超过结温。但是如何才能评估出芯片表面的温度呢,TI是否有相关文档呢?

2、有哪些可以缓解电路板温度高的措施呢?

非常感谢!