This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA309:我在使用USB_DAQ校准中使用钳位和并行使用2块板出现的一些问题

Part Number: PGA309

EEPROM.txt
Fullscreen
1
2
5449_0000_0103_0597_D31F_007F_1703_BA7B_2941_4B79_99FF_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_2941_0000_0000_7FFF_0000_DD37
5449_0000_0103_0594_C41F_0047_1703_C9B6_2932_6801_8ED3_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_2932_0000_0000_7FFF_0000_CCDA
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX
Tio332_240125_145719.log

hello.
I'm calibrating the PGA309 with a USB-DAQ board and I'm experiencing two problems
1. The output of PGA309 is 0.5-4.5V analog output, but when I use register R5 for clamping, the lower clamp can reach 0.21V or so.
But the upper clamp only goes up to about 4.04V. The range I want to use is 4.5V, and the upper clamp should be greater than the 4.5V operating value. For example, if VREF is 4.096V and R5 is set to HEX47, the output will have a lower clamp of 0.21V and an upper clamp of 4.02V. 2;
2. now with two USB-DAQ boards respectively set the jumper cap address 2F90, 2F91, parallel operation will appear 2F90 read and write no problem but 2F91 read and write will often unsuccessful situation, I made a copy of the Tio32.dll folder and renamed it for the use of the 2F91 thread.
I am looking forward to your reply! Attached are the EEPROM values for some products

麻烦为我转发一下,我还为获得英文论坛的权限。十分感谢!

  • 非常感谢您的帮助

  • 不用谢

  • 收到如下英文论坛回复:

    1. The PGA309 over and under scale limit is designed to be a ratio of the reference voltage Vref (see user's guide PGA309 user's guide section 2.9).  Thus, if a 4.096V reference is used the maximum clamp is 4.096V * 0.9708 = 3.976V.  If a 5V external reference is used the clamp can be 5V * 0.9708 = 4.85V.  I believe that this feature was mainly intended for use with an ADC where the ADC reference is shared with the PGA309 reference.  This way the PGA309 output never exceeds the ADC reference voltage.  If you want a clamp that allows for 0.5V to 4.5V you will need to use an external reference.
    2. I do not believe that the PGA309EVM software allows for two EVM to be run at the same time.  The address select option is used to select the USB HID product ID.  The software automatically scans the four available product ID to see if one is present, and will attempt communications if it finds one.  I am not sure I understand your question.  Are you successfully communicating with two devices at once?  I suggest if you want to calibrate multiple sensors at once you use the MULTI-CAL-SYSTEM 

    I hope this helps.  Best regards, Art Kay

    若需要跟进请说明,我会继续协助转发到英文论坛。

  • Thank you for your answers.
    I have some more questions;
    1. regarding the clamp being located on the internal reference, I reviewed the information in your guide and my understanding is that to achieve the operating conditions I need (other than 0.5-4.5V) I need to make a change to the product (the PGA309 sensor) and I need to connect the 5V from the VS to the 12PIN of the 309 and set D10D8 in R3 to zero.
    2. When calibrating the 309 on two USB-DAQ boards in parallel, I developed a software to do this using TIO32.DLL provided by TI, and this has caused some problems during the work, and just yesterday I reconnected JUMP8 on one of the boards to GND, and found that the problem has magically improved a lot, and I don't understand what is going on here, and I looked at the manual for information that JUMP8 is a One-Wire accelerated circuit, and that it is a one-wire accelerated circuit. I read in the manual that JUMP8 is a One-Wire accelerated circuit and it was connected to SPD when I had the problem before. Also, I would like to ask if I have to enable the acceleration circuit if I add a 100pF capacitor to the OUT pin in 3-wire mode?
    Again, I look forward to your reply!

    再次感谢您的帮助,以上是我的一些问题,麻烦您了

  • 已将您的问题提交到英文论坛。

  • 英文论坛回复:

    1. You will need to connect pin 16 on the PGA309 (Vref) to 5V.  One option is to connect Vs (Pin 3) to Vref (pin 16).  However, Vs is often has drift an noise when compared to a precision voltage reference.  This may be ok if you are doing a ratiometric design.  That is, the voltage reference connected to the PGA309 is also connected to the ADC that is reading the PGA309 output.  Using the ratiometric approach, when the reference shifts the PGA output will shift by the same percentage, and the ADC input range (LSB size) will also shift by the same percentage.  Thus the shift will cancel out.  On the other hand, if you expect the output to have absolute accuracy, you should use an external 5V voltage reference on pin 16. 
      1. I do not understand your comment regarding "D10D8 in R3 to zero."  I do not see this component on the PGA309EVM test board.
      2. Your comment regarding pin 12 of the PGA309 does not seem correct.  This is the PRG pin and is used for digital communications.  It would not make sense to connect Vs directly to the PRG pin.
    2. The "one-wire speed up circuit" JUMP8 is generally recommended to be turned on for all PGA309 operation.  In fact, I do not believe I have every used this in the off position.  It is especially important to use this when long cables are used.  The purpose of the circuit is to add a current boost on the one-wire digital signal to make the rise time faster.  This reduces the possibility of data communications issues from slow rise time.  The circuit works effectively on the EVM to drive a 10nF capacitor so you should not have issues with 100pF.

    I hope this information is useful for you. 

  • 这些信息非常有帮助,同时也感谢您的帮助,我接下来将对这些问题进行讨论和修改。

    关于1.a 这个我是想说的是R3中的 D8和D10。

              b REFin/out是16PIN 是我看错了

    再次感谢您的帮助