This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6525: How to calculate the input current ?

Part Number: LMH6525

INPUTS

Current-Setting Inputs

The 4 input channels are transconductance-type inputs. This means the output current of the channel is

proportional to the current (not voltage) sourced into the input pin. That is why these pins are designated by the

letter “I” to indicate the current input nature of the pin. The read channel current-setting pin is “IR”, the Channel 2

current-setting pin is “I2” and so on. Using a transconductance-type input eliminates the high-impedance inputs

associated with a voltage input amplifier. The lower input impedances of the input nodes lowers the susceptibility

of the part to EMI/RFI. The Read Channel (IR) and Channel 3 (I3) and 4 (I4) current-setting inputs have a gain of

  1. The Channel 2 input (I2) has a current gain of 300. Sourcing one milliampere into the pins IR, I3 or I4, will

result in 150 mA at the output for each Channel, while 1 mA into I2 will result in 300 mA at the output for Channel

  1. These currents of 150 mA and 300 mA are the maximum allowable currents per channel. The total allowable

output current from all the channels operating together exceeds 500 mA.

         How to calculate the input current ?

x 出现错误。请重试或与管理员联系。