This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于OPA2614的使用

Other Parts Discussed in Thread: OPA2614

大家好,我想请教个问题。电路图如下,输入信号为500mV幅值的正弦信号,频率1kHz,OPA2614的6脚出来的信号为500mV峰峰值正弦波,按照电路设计应该是放大两倍;由于使用了单电源12V,输出带6V的偏置,为了滤除偏置后端加了电容,但为了防止容性负载过大导致相位出问题,串了一个电阻,原本设计希望,经过电容后的1V峰峰值信号,叠加一个2.5V(图中应该是R2---4k,R5---1k)的静态工作点,经过一个由2SC1971 RF功放构成的射极跟随器,在R6得到一个在一定直流偏置上叠加交流信号,但出来的信号只有几十mV的峰峰值,应该怎么去分析解决呢?

  • 亲;放大器即可以放大交流信号也可以放大直流信号。因此;放大器的正负极都需要偏置!对于你的电路;建议将C1移至R3右侧。

  • 谢谢你的回答,你指的应该是C1放到R9的右边吧,放到R3右边算什么,还有应该怎么理解C1在R9左边和右边的不同?我其实最想知道的是R4和C5的取值,现在是输出不对,运放负输入和我信号源是一样的,没问题

  • 亲;正因为运放负输入与信号源一样;但是!!!!但是!!!!你的正端是直流信号!你的放大器两输入端的差值(差模信号)不仅有信号源信号还有两端直流信号!!!!!!!!!这是最主要的问题;其它都是次要的!R4C5不至于影响波形形状!

    挪C1的目的就是将直流信号隔离成共模信号!

  • 这是官方datasheet给的单电源解法,C1放在R9左侧和右侧会带来什么影响呢,怎么就能把差模信号的直流量去掉了?

  • 亲;放左侧;放大器负输入通过RG/RM,直流接地,直流放大倍数为(RF+RG+RM//RI//电容内阻)/(RG+RM)。若电容直流阻抗为无穷大,直流放大倍数为(RF+RG+RM)/(RG+RM)。按图4,直流放大倍数为3。按图正输入2.5V;放大器直流分量输出为约5V(饱和输出)。

    电容放R9右侧,直流放大倍数为(RF+RG+电容内阻)/(RG+RG//RI+电容内阻),直流放大倍数为1。按图4;直流分量输出2.5V。

    这就是电容不同位置的区别。

  • 非常感谢,鄙人受教了,以前设计运放电路没考虑过直流放大倍数,认为和交流一样,之前看过一些文章,说是C1放在R9右侧在分析直流回路时会产生一个悬浮地,所以没这么用。你看电路图中后端的设计合不合理,就是运放6脚到RF功放电路的,大电流一直出不来

  • 亲;R4可能有点偏大,建议减小到100ohm左右试试。

  • 你好,电路改动后,输入1k 500mV幅值的信号,2614的6脚输出为420mV,同时R2与R5交点处波形电压为:2.4V直流偏置,350mV峰峰值的1k信号

  • 偏置电压不对,如果只需要放大连续的交流信号,可以使用交流放大器,将R9去掉,然后匹配一下阻抗即可。

  • 您看下我的逻辑对不对:电路改动如上,我原本想法是,输入信号可能含有只留分量,在放大之前我先滤除它,由于采用单电源+12V工作,所以运放6脚有6V的偏置对吧,再经过输出电容C5,把直流分量去除,这时候用R2和R5为三极管提供一个2.4V静态工作点。但是为什么我输入信号是1k,500mV幅值的正弦波,过了C5之后只有350mV了

  • 最新提问如11楼,希望大家给些建议

  • 请问500mV是哪里测量到的,理论上输入电压的大小为R3和C1之间的电压值。

    还有R1R3的值太小了,请使用千欧级的电阻,测量放大器是否正常,请观察R4左边的电压信号。测量三极管B级的信号,由于三极管的输入阻抗比较低会有影响。

    1. 500mV是信号发生器的数值,R1和R3是根据手册上的大小来选得,一般CFA不都是根据手册推荐值让其工作在最佳状态吗?后级的三极管带不起来(没正常放大)

x 出现错误。请重试或与管理员联系。