This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,我想请教个问题。电路图如下,输入信号为500mV幅值的正弦信号,频率1kHz,OPA2614的6脚出来的信号为500mV峰峰值正弦波,按照电路设计应该是放大两倍;由于使用了单电源12V,输出带6V的偏置,为了滤除偏置后端加了电容,但为了防止容性负载过大导致相位出问题,串了一个电阻,原本设计希望,经过电容后的1V峰峰值信号,叠加一个2.5V(图中应该是R2---4k,R5---1k)的静态工作点,经过一个由2SC1971 RF功放构成的射极跟随器,在R6得到一个在一定直流偏置上叠加交流信号,但出来的信号只有几十mV的峰峰值,应该怎么去分析解决呢?
谢谢你的回答,你指的应该是C1放到R9的右边吧,放到R3右边算什么,还有应该怎么理解C1在R9左边和右边的不同?我其实最想知道的是R4和C5的取值,现在是输出不对,运放负输入和我信号源是一样的,没问题
亲;正因为运放负输入与信号源一样;但是!!!!但是!!!!你的正端是直流信号!你的放大器两输入端的差值(差模信号)不仅有信号源信号还有两端直流信号!!!!!!!!!这是最主要的问题;其它都是次要的!R4C5不至于影响波形形状!
挪C1的目的就是将直流信号隔离成共模信号!
偏置电压不对,如果只需要放大连续的交流信号,可以使用交流放大器,将R9去掉,然后匹配一下阻抗即可。
请问500mV是哪里测量到的,理论上输入电压的大小为R3和C1之间的电压值。
还有R1R3的值太小了,请使用千欧级的电阻,测量放大器是否正常,请观察R4左边的电压信号。测量三极管B级的信号,由于三极管的输入阻抗比较低会有影响。