ti的工程师:
我这里有一个工程,同时要使能AIC3204的ADC和DAC,IIS总线接的是6748,这里双向通信我们之前检测是没有问题的。AIC3204电路如下
我们目前数字信号从DIN输入后,LOL和LOR有模拟信号输出。AIN-1、AIN+1模拟信号输入,但是DOUT数字信号一直没反应。我改了好几遍偏置一直没啥反应请ti的工程师看看是不是哪里配置的有问题。
void aic3204Init(void)
{
CODEC_RESET = 1;
delay_ms(2);
CODEC_RESET = 0;
//;p Reset 1 # Release the reset pin
//;# RESET
aic3204_res = aic3204_Write_Reg(0x00,0X0); //WW 30, 00h, 00h ; # Select register page 0
aic3204_res = aic3204_Write_Reg(0x01,0X1); //WW 30, 01h, 01h ; # I2C reset
delay_ms(10);
//;# CLOCK SETTINGS
aic3204_res = aic3204_Write_Reg(0x0B,0X81); //WW 30, 0Bh, 81h ; # PoWWer up the NDAC divider WWith value 1
aic3204_res = aic3204_Write_Reg(0x0C,0X82); //WW 30, 0Ch, 82h ; # PoWWer up the MDAC divider WWith value 2
aic3204_res = aic3204_Write_Reg(0x0D,0X00); //WW 30, 0Dh, 00h ; # Program OSR for DAC to 128 (MSB)
aic3204_res = aic3204_Write_Reg(0x0E,0X80); //WW 30, 0Eh, 80h ; # Program OSR for DAC to 128 (LSB)
//12 13 14
//w 30 12h 81 # Power up the NADC divider with value 1
//w 30 13h 82 # Power up the MADC divider with value 2
//w 30 14h 80 # Program OSR for ADC to 128
aic3204_res = aic3204_Write_Reg(0x12,0X81);
aic3204_res = aic3204_Write_Reg(0x13,0X82);
aic3204_res = aic3204_Write_Reg(0x14,0X80);
//;# DIGITAL INTERFACE
aic3204_res = aic3204_Write_Reg(0x1B,0X00); //WW 30, 1Bh, 00h ; # I2S, 16-bit, BCLK and WWCLK are inputs
//;# PROCESSING BLOCK USAGE
aic3204_res = aic3204_Write_Reg(0x3C,0X08); //WW 30, 3Ch, 08h ; # Select DAC processing block PRB_P8
//w 30 3D 04 # Select ADC processing block PRB_R4
aic3204_res = aic3204_Write_Reg(0x3D,0X04);
//;# ANALOG POWWER SUPPLY
aic3204_res = aic3204_Write_Reg(0x00,0X01); //WW 30, 00h, 01h ; # Select register page 1
aic3204_res = aic3204_Write_Reg(0x01,0X08); //WW 30, 01h, 08h ; # Disable internal crude AVDD before poWWering up the internal AVDD LDO
aic3204_res = aic3204_Write_Reg(0x02,0X01); //WW 30, 02h, 01h ; # Enable internal analog LDO, analog blocks poWWered
//;WW 30, 02h, 00h ; # Enable internal analog LDO, analog blocks poWWered
aic3204_res = aic3204_Write_Reg(0x0A,0X40); //WW 30, 0Ah, 40h ; # Common mode set to 0.75V
//;# MICPGA DELAY, REFERENCE CHARGING AND HEADPHONE DE-POP
//;WW 30, 47h, 31h ; # MICPGA startup delay is 3 ms
aic3204_res = aic3204_Write_Reg(0x7B,0X01); //WW 30, 7Bh, 01H ; # Reference charging time is 40 ms
//aic3204_res = aic3204_Write_Reg(0x14,0X65); //;WW 30, 14h, 65h ; # HP driver poWWer-up: 50 ms soft routing step time, 5.0 time constants, 6k resistance
//;# AUDIO ROUTING
//aic3204_res = aic3204_Write_Reg(0x0C,0X08); //;WW 30, 0Ch, 08h ; # HPL routing: Left channel
//aic3204_res = aic3204_Write_Reg(0x0D,0X08); //;WW 30, 0Dh, 08h ; # HPR routing: Right channel
aic3204_res = aic3204_Write_Reg(0x0E,0X08); //WW 30, 0Eh, 08h ; # LOL routing: Left channel
aic3204_res = aic3204_Write_Reg(0x0F,0X08); //WW 30, 0Fh, 08h ; # LOR routing: Right channel
//Full-Differential Mono Mic connected to IN1L/IN1R select page 1
//w 30 34 00 # No routed to Left MICPGA Positive
//w 30 36 00 # No routed to Left MICPGA Negative
//w 30 37 40 # IN1R is routed to Right MICPGA Positive with 10K resistance
//w 30 39 10 # IN1L is routed to Right MICPGA Negative with 10K resistance
aic3204_res = aic3204_Write_Reg(0x34,0X00);
aic3204_res = aic3204_Write_Reg(0x36,0X00);
aic3204_res = aic3204_Write_Reg(0x37,0X40);
aic3204_res = aic3204_Write_Reg(0x39,0X10);
aic3204_res = aic3204_Write_Reg(0x12,0X00); //WW 30, 12h, 00h ; # LOL driver is not muted
aic3204_res = aic3204_Write_Reg(0x13,0X00); //WW 30, 13h, 00h ; # LOR driver is not muted
aic3204_res = aic3204_Write_Reg(0x09,0X3C); //WW 30, 09h, 3Ch ; # Output Driver Power Control ALLOUT powered up
delay_ms(10);
//mov A,28h ;after 18 cmds do delay 8.6ms
//call dly_lcd_timex
aic3204_res = aic3204_Write_Reg(0x00,0X00); //WW 30, 00h, 00h ; # Select register page 0
aic3204_res = aic3204_Write_Reg(0x3F,0X0D6); //WW 30, 3Fh, 0D6h ; #
aic3204_res = aic3204_Write_Reg(0x40,0X00); //WW 30, 40h, 00h ; #
}