This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
PCM2906C ,spdif out 及 3.5mm音频输出口 功能正常, spdif in 无功能 ?何解
晶振 供电也都正常..,示波器量过 信号有输入 芯片24脚 ,并且从24脚通过引线方式到 spdif接口 音响, 音响声音是正常的 ,测试环境就是 产品通过 usb接win7电脑,产品的spdif in 接口 接另外一个标准spdif out信号 , 在win7 录音界面 看录音功能 ,无功能
数据格式没问题 ,分别验证过 16位 ,32K 44.1K 48K的输入 ,并且幅度也调整到PCM2906C要求的幅度(低0 ,高3.3v) ,仍旧是没有功能, 但也有看到规格书21页 This feature is a customer option. It is the responsibility of the user to implement this feature ,有这么一句 ,不明白它想说明说明个意思?