This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

(TAS5805M)two speaker output volume is small 双喇叭输出声音小

Other Parts Discussed in Thread: TAS5805M

    First we use 1 speaker output ,sound(volume) is OK.But when we change hardware to BTL mode and use 2 speaker output, sound(volume) is very small.Even i change the volume to max (change from 100->144),it also small.But we check the signal,the amplitude is OK,about 10V 

开始我们是采用单speaker输出的,PBTL,这个状态下播放音乐音量是正常的。但是我们修改了硬件为BTL模式,采用双喇叭输出,软件没有改变。此时输出的音量非常小,即使我们把默认音量由100调整到144,依然是很小。但是用示波器看信号幅度是足够的,峰峰值大概有10V左右了。

check the parameter,i found register 02 is set to 0,that is PBTL .

查看寄存器,发现register 02的值是为0的,就是说还是PBTL的模式,没有变更为BTL的模式。

Please send us BTL mode parameter list,which parameter (register value)we need to change?

请帮忙提供BTL模式的参数列表,即有单喇叭变成双喇叭需要修改哪些寄存器的值?

  • 您好,
    TAS5805M在BTL模式下要求的最小负载与PBTL模式下是不一样的(参考数据手册7.3 Recommended Operating Conditions),在BTL模式下您外接的两个喇叭阻抗是多少呢
  • 请问您方便提供原理图吗? 或者您使用的是TI EVM?

    建议您参考数据表的第48页来配置BTL模式:

    w 58 00 00 //page 0

    w 58 7f 00 //book 0

    w 58 02 00 // BTL, BD mode and Fsw-768KHz

    注意:0x58是I2C地址。

    建议使用TI的PPC3工具进行调试,因为它包含所有必要的寄存器设置。
  • Dear Amy:

             目前我们接的两个喇叭都是4欧 15W的,是符合最低要求的。PVDD 12V,电感用的4.7uH。

             但是我看寄存器,目前寄存器02的设定是04,也就是说PBTL mode。我改成0,反而没有声音出来,这是比较奇怪的。

             另外,用示波器看波形,我们播放1k0db的正弦波,量喇叭接座,+ 极是正确的正弦波波形(叠加了直流电平在上面),但是 - 极类似与杂波(很密集的杂乱波形,幅度是10V左右)。这个现象有没有听说过?

  • 当前原理图如下:电源部分用12V和1.8V

  • 您好,您将FSW_SEL设置为384KHZ,即register 02设置为0x10试一下。
    检查一下电感是不是好的,图中所选电感过电流太小了,至少选择大于3.32A的电感。
  • 感谢各位的大力支持。目前修改寄存器为BTL之后,FSW_SEL 为 384k 就OK了。