This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

(TAS5805M)two speaker output volume is small 双喇叭输出声音小

Other Parts Discussed in Thread: TAS5805M

    First we use 1 speaker output ,sound(volume) is OK.But when we change hardware to BTL mode and use 2 speaker output, sound(volume) is very small.Even i change the volume to max (change from 100->144),it also small.But we check the signal,the amplitude is OK,about 10V 

开始我们是采用单speaker输出的,PBTL,这个状态下播放音乐音量是正常的。但是我们修改了硬件为BTL模式,采用双喇叭输出,软件没有改变。此时输出的音量非常小,即使我们把默认音量由100调整到144,依然是很小。但是用示波器看信号幅度是足够的,峰峰值大概有10V左右了。

check the parameter,i found register 02 is set to 0,that is PBTL .

查看寄存器,发现register 02的值是为0的,就是说还是PBTL的模式,没有变更为BTL的模式。

Please send us BTL mode parameter list,which parameter (register value)we need to change?

请帮忙提供BTL模式的参数列表,即有单喇叭变成双喇叭需要修改哪些寄存器的值?