This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC3104 MIC2 单端输入模拟信号, right adc 没有数据到DSP

config  init code

 

aic3104_register_write(101, 0x00); ///  CODEC_CLKIN uses PLLDIV_OUT

 

aic3104_register_write(3, 0x93); //// PLL enable, PLL Q value: 2 ,PLL P value: 3

aic3104_register_write(4, (0x04<<2) & 0xfc); //// PLL J value: 4

aic3104_register_write(5, ((0 << 2)>>8) & 0xff); /// PLL D value: (0  *4) /  256

aic3104_register_write(6, (0 << 2) & 0xff); //// PLL D value: (0  *4) %  256

aic3104_register_write(11, 0x04); //// PLL R value: 4

 

aic3104_register_write(8,0xD0);

aic3104_register_write(9,0x47); //// DSP mode

 

aic3104_register_write(2, 0xAA); //// ADC and DAC fs, delate this for 48K, use this for 8K

 

aic3104_register_write(17, 0xFF);

aic3104_register_write(18, 0xFF);

aic3104_register_write(19, 0x78);

aic3104_register_write(21, 0x78);

aic3104_register_write(22, 0x78);

aic3104_register_write(24, 0x78);

 

aic3104_register_write(26, 0x00);

aic3104_register_write(28, 0x00);

aic3104_register_write(29, 0x00);

aic3104_register_write(31, 0x00);

 

aic3104_register_write(32, 0x00);

aic3104_register_write(33, 0x00);

 

aic3104_register_write(15, 0x00);

aic3104_register_write(16, 0x00);

 

// aic3104_register_write(25, 0x80);   

aic3104_register_write(7, 0x0C);

aic3104_register_write(37, 0xC0);

aic3104_register_write(43, 0x00);

aic3104_register_write(44, 0x00);

aic3104_register_write(82, 0x80); ////  DAC_L1 is routed to LEFT_LOP/M.

aic3104_register_write(86, 0x8B);

Open mic2R to right adc

 

aic3104_register_write(7, 0x00);

aic3104_register_write(37, 0x00);

 

aic3104_register_write(82, 0x00);

aic3104_register_write(86, 0x02);

 

aic3104_clear_bits(37, 0x40);

aic3104_register_write(18, 0xF0);

aic3104_register_write(22, 0x7C);

 

这样测试dsp是没有数据的。3104MIC2.doc