Part Number: PCM6360-Q1
您好
在使用6360的时候,bais 不需要给MIC 偏置供电的时候,下面2个PIN 可以悬空么?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,如果不使用MIC偏置的话,可以将HVDD和AVDD接在一起,或者接外部供电源(外部接电源需要小于10V或者大于等于AVDD)。
而MICBIAS作为输入引脚,也不 建议悬空,建议参考datasheet中的AC耦合模式连接。
因为MICBIAS这个功能可以通过寄存器将其配置为power down,所以您也可以正常连接,只是将其配置为power down模式就好。