This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM6360-Q1: VBAT_IN 电源供电

Part Number: PCM6360-Q1

你好

我在使用PCM6xx0-Q1的时候,VBAT_IN没有供电,Microphone Faults我也不需要检测,下面4个功能需要VBAT_IN 的供电么?我用PPC软件没有找到下面4个诊断对应的设置,还请帮忙看一下 感谢

MICBIAS Overvoltage 

MICBIAS Overcurrent

MICBIAS Load Current

Overtemperature Fault

  • 您好,VBAT_IN是输入诊断电路供电电压,如果不需要输入诊断功能 ,可将VBAT_IN直接接GND防止漏电流的产生。

    您指的MICBIAS Overvoltage  等这几个配置,都是micbias偏置电路,是HVDD供电电压,如果这几个诊断也不需要的话,HVDD接到或者低于10V , 高于或等于AVDD的电压。

  • 我需要上面4个诊断的话也可以把VBAT_IN直接接GND么?

    谢谢

  • VBAT_IN是针对输入诊断电路的,而上述三个诊断都是针对micbias电路的,如果需要上述诊断,是需要启动micbias电路也即是需要HVDD电压的。

    所以我认为如果上述三个micbias诊断需要的话, 而不需要输入诊断,VBAT_IN 是不需要的,可以将其就接地。

    过温保护Overtemperature Fault不是单纯的micbias电路或者输入诊断部分的,是整个芯片的结温超过多少度引起的保护,所以VBAT_IN是可以接地的。

    总的来说,如果不需要输入诊断功能,VBAT_IN 是可以悬空或者可以接地的,接地则是为了防止漏电流的产生。