This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3116D2: 输出强度突然变弱

Part Number: TPA3116D2
  1. 原理图如pdf文件,其中R9,R18改成75KΩ,R10,R19改成47KΩ,也就是增益从26dB改成36dB。
  2. Layout如PCB文件
  3. 电源使用DC24V/5A
  4. 声音调到最大,工作一段时间,出现问题如下:
  • 一个产品,开到最大音量,几分钟后会出现其中一个TPA3116D2输出的两路输出强度变低。用万用表AC档量喇叭两端电压,正常工作的喇叭两端电压是6V左右,强度变低的喇叭两端的电压只有3V左右。而且强度变低的TPA3116D2输出一直保持低,只有断电重新上电才恢复。正常输出的TPA3116D2上的散热片温度大概120℃,变低的TPA3116D2上的散热片温度大概80℃。
  • 一个产品,工作一段时间(十几分钟左右),两个TPA3116D2 IC输出的强度交替变低,变高。

请帮忙分析原因。谢谢!

x 出现错误。请重试或与管理员联系。