TPA3110D2输出声音很小,测试输出占空比50%左右,一直没有什么变化,请问是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
哦哦,我没注意看您这里加了RC低通滤波器,这里的截止频率159HZ确实太低了把有效音频信号都衰减掉了,使得输出声音很小。需要减小R和C的值将截止频率调高些。
但是R1和R12的阻值得不一致,是因为我走线的原因导致阻抗不一致吗?
这里您想表达什么意思?我没看明白
是的,差分输入前端加的RC电路应该是一致的。在差分输入时,首先需要您确认的是差分输入幅值是多少?如果INP和INN管脚输入信号是一样的,那么差分输入是0,输出就没有声音。
另一个需要注意的是RC滤波电路的截止频率,不能衰减掉有效音频信号,之前您使用的参数R=1KΩ,C=1uF,形成的截止频率太低了会将音频信号衰减掉,也会造成输出声音很小。
但是正负PIN上接的阻值不一致才能将声音调大,想问是不是原先差分阻抗不一致,加了不同阻值后一致了,得有一定压差才能满足要求
阻值一致时,差分输入的正负端电压分别是多少?看您的描述像是差分输入的正负端电压一样了,没有压差了?没有压差差分输入就是0,输出就没有声音。差分输入的有效信号就是正负输入端的压差。