Part Number: LMK00334
Other Parts Discussed in Thread: LMKDB1104, LMK6H,
您好!
晶振100M产生的时钟,分别给SOC PCIE30 REFCLK和M.2 NVME硬盘接口使用,请帮忙检查原理图:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
VBB需要接近VOPP/2*0.5---配置在LMK00334芯片的哪个管脚?没看到手册手册里有具体说明
您将未使用的支路偏置在从CMOS驱动器侧的LMK输入看到的输入摆动的中点。---这句话意思是例如我的原理图需要将没用到的芯片12、14、15、26和27输入管脚,需要偏执到VBB?
您好!
我发现我上面理解错了,我把OSCin和CLKinX理解成同一个东西了,其实不是,我重新看了手册里面对OSCin解释,确实是只说了AC耦合方式,但是确实我看到EVM里面是没有用AC耦合,就是直接输入,但没对SMA_OSCin做出一些解释。当初我的原理图里面R355是没有焊接,导致后面CLKout的占空比不对了,看手册里面说有内部基准电压,但是好像没看到OSCin输入电压的要求,所以当时看到CLKinX的直流耦合要分压,所以我就直接分压了,发现占空比也对了,看到我的用法手册里面没有提到也没有具体说对OSCin输入要求,所以想要了解下,我这样(OSCin输出直接串49.9Ω加下拉49.9Ω)使用是不是可行,有没什么弊端?