This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8860: ADS8860 for IRIG-B AMdecode

Part Number: ADS8860


We are designing an IRIG-B  AM demodulation circuit. The input signal is IRIG-B AM, the amplitude is peak-to-peak 0.5V to 12V, and the modulation ratio is 6:1 to 2:1. In order to extract the time information from the IRIG-B AM signal, we need to do AD conversion. But The input signal has a very wide range of variation .How to design the front-end circuit for ADC(ADS8860).

  • 您好,

    收到了您的案例,调查需要些时间,感您的耐心等待。

  • Hi,

    Thanks for your post. What is your end equipment?

    The input circuit will depend on the maximum and minimum input voltage. Could you let me know what these values are after modulation? What max and min voltages will the ADC input see?

    If the range is large, the smaller voltages will not be very high resolution measurements. One simple method of stepping down voltage is shown in the circuit cookbook on page 45 here. Page 50 shows another option.

  • Thanks for your replay.Our equipment is based Zynq SoC.I reviewed the spec again,the Input level (high amplitude modulation) is -20dBm to +6dBm.Impedance: 600 ohms balanced.

  • Hi,

    Thanks for the feedback! Input levels in dBm are relative. It would be helpful to have the full signal range to the ADC input in volts. For now, I will assume it is peak-to-peak 0.5V to 12V = 12V-0.5V = 11.5Vpp, as you mentioned in your first post. Please let me know if my understanding is incorrect. The 11.5Vpp input is larger than the ADS8860's 0V-5V input range, the input will need to be divided down. The use of a (for example) 10kohm equivalent resistor divider + the 600 ohms input impedance will not allow the internal sample and hold capacitor to settle within the acquisition time and would reduce the sampling rate to about ~8ksps, as shown below through use of the Analog Engineer's calculator:

    As a result, the customer will need a driver amplifier to drive the ADC inputs. One such example is shown in the datasheet, figure 64. The customer can size the feedback resistors to divide down the input. Since this is an inverting gain amplifier configuration, a common-mode voltage is shown at the positive input of the amplifier to bring the input back within the positive 0V to 5V range. You can size your resistors as Rf = 1kohm and R1 = ~2.5kohm to allow the 11.5Vpp signal to become 4.6Vpp (-0.2V to -4.8V). You can add a 5V common-mode to the amplifier positive input to shift this voltage up to 0.2V to 4.8V to stay within the ADC's input range. 

    I did not go into much detail on how this op-amp was selected as the text describes that. I calculated what the minimum amplifier gain-bandwidth product (GBW) needed to be to drive this 1MSPS ADC. Other amplifiers of similar GBW and distortion may be used as well.

    I hope this helps,

    Best regards,

  • about ADS8860.pdfThank you for your reply. In the attached document, I re-described the characteristics of our signal.

  • Hi,

    Thanks! So it sounds like the minimum input = 109.6mV/6 = 18.27mV and the max input is 21.189/2 = 1.0945V. A gain of ~4.5 would be good to gain the 1.0945V to within the 5V input range. However, the stability and noise from the amplifier will have to minimal as well. Perhaps a driver amp in noninverting configuration like this: https://www.ti.com/lit/an/sboa271a/sboa271a.pdf

    I am looping in the amps team to help with a suitable gain stage.

    Best regards,

  • Hello Eric,

    I want to ensure that I know that I know the input signal properly.

    amplitude is peak-to-peak 0.5V to 12V, and the modulation ratio is 6:1 to 2:1.

    The minimum 0.5Vpp for high bit and (0.5V/6) = 0.83Vpp for low bit

    The maximum 12Vpp for high bit and (12V/2) = 6Vpp for low bit

    Frequency is 1kHz

    It would be fine for a delay for automatic gain control to normalize the input signal.

    The input signal sources are wildly variable in amplitude, but each source is fairly consistent in levels.