We are designing an IRIG-B AM demodulation circuit. The input signal is IRIG-B AM, the amplitude is peak-to-peak 0.5V to 12V, and the modulation ratio is 6:1 to 2:1. In order to extract the time information from the IRIG-B AM signal, we need to do AD conversion. But The input signal has a very wide range of variation .How to design the front-end circuit for ADC(ADS8860).