Part Number: ADC3664

您好!在使用ADC36664时,进行内部NCO数字混频低通滤波之后,发现A、B两个通道的信号相位反相,相差约180度,我想了解一下A、B两通道的混频源是否是独立的,或者是同源但是相位相差180度。如图1所示,1、2分别为通道A的实部和虚部,3、4分别为通道B的实部和虚部。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
对于 DDC A 和 DDC B,有两个独立的 NCO。分享您的原理图和寄存器配置可能会有所帮助,这样我们可以帮助您排查此问题。

我们现在不是使用的是fs/4混频的方式,我的寄存器配置为2线制、14位、按4倍复杂抽取,采样率为100M,采样信号的频率(点频实信号)是41MHz,混频信号为40MHz,抽取之后我们的采样率为25M,但是我现在这个结果就是发现,AB两个通道的寄存器设置的模式都是一样的,但是对于同样一个信号AB两个通道输出的信号相位差了180°,这个图中,第一个信号和第二个信号分别为AB两个通道的实部,第三个信号和第四个信号分别为AB两个通道的虚部,可以看出这两个通道相位差了180°,但是两个通道我给的信号都是同样一个信号。想问一下,出现这个问题的原因是什么?