Part Number: ADS8685W
我们现在使用ADS8685W进行采样,现在遇到的问题的采集精度很不好。用一节南孚电池直接作为信号输入送入到ADC进行采集,电路板上的其他前端电路都断开了,这时采集的值也会有6个mV以上的波动。
具体见附件,请帮忙解答,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS8685W
我们现在使用ADS8685W进行采样,现在遇到的问题的采集精度很不好。用一节南孚电池直接作为信号输入送入到ADC进行采集,电路板上的其他前端电路都断开了,这时采集的值也会有6个mV以上的波动。
具体见附件,请帮忙解答,谢谢。
您好
能否请确认数字通信时序是否符合第5.6节“时序要求”中的限制范围?

在示波器上以及使用4MHz时钟时都难以观测。我需要确认所测量的噪声并非仅为数据读取偏移所致。
您能否也告知设备配置的功率范围?电池输出功率范围是多少?它是如何与设备连接的(松散导线还是直接物理接口)?
最后,关于物资实际配置的两个关键问题:
该原理图中有两个VCC电源,一个为U208的输入端,另一个通过R412(10欧姆)连接至V3V3-3,哪一个用于ADC的AVDD供电?
ADS8685W需要AVDD电压高于4.75V。
DVDD可设为3.3V,这没问题,但在示波器图像中,数字信号的电压水平似乎约为5V。DVDD的设定值是多少?
当AVDD为5V时,DVDD也可以是5V,这不成问题。我只是想确认一下。
此外,请确认用于与ADC通信的控制器的供电电压、高电平/低电平输入输出电压以及高电平/低电平输入电压的具体数值?