This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8685W: ADS8685W采样精度问题

Part Number: ADS8685W

我们现在使用ADS8685W进行采样,现在遇到的问题的采集精度很不好。用一节南孚电池直接作为信号输入送入到ADC进行采集,电路板上的其他前端电路都断开了,这时采集的值也会有6mV以上的波动。

具体见附件,请帮忙解答,谢谢。

ADS8685W.docx

  • 已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 您好

    能否请确认数字通信时序是否符合第5.6节“时序要求”中的限制范围?

    在示波器上以及使用4MHz时钟时都难以观测。我需要确认所测量的噪声并非仅为数据读取偏移所致。

    您能否也告知设备配置的功率范围?电池输出功率范围是多少?它是如何与设备连接的(松散导线还是直接物理接口)?

    最后,关于物资实际配置的两个关键问题:

    该原理图中有两个VCC电源,一个为U208的输入端,另一个通过R412(10欧姆)连接至V3V3-3,哪一个用于ADC的AVDD供电?
    ADS8685W需要AVDD电压高于4.75V。
    DVDD可设为3.3V,这没问题,但在示波器图像中,数字信号的电压水平似乎约为5V。DVDD的设定值是多少?
    当AVDD为5V时,DVDD也可以是5V,这不成问题。我只是想确认一下。
    此外,请确认用于与ADC通信的控制器的供电电压、高电平/低电平输入输出电压以及高电平/低电平输入电压的具体数值?

  • 原本电路中ADC芯片的SPI逻辑电平使用的是3.3V的,MCU使用的是5V的,现在我已经更换了芯片,同时将ADC芯片的DVDD更换为5V电平。数字通信时序符合限制范围。电池通道松散导线与设备连接,此应用中电池无负载,直接通过ADC芯片测试电池的电压

  • 1,符合时序要求。2,电池本身无负载,只做过ADC芯片的模拟输入提供稳定的电压源,通过松散导线连接到设备。3,原本电路中MCU使用的是5V电平,DVDD是3.3V电平,现已经将DVDD的电平更换为与MCU相同的5V电平,再进行测试,精度依然很差