This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DS90UB914A I2C不通问题



您好

          我将913A和914A两块PCB用同轴连接在一起。两块PCB板子的原理图如附件913A是M1_0605   914A是M2_0605.

         913A目前mode是外部晶振供电贴的是R11 4.7K电阻。贴了U12外部48M晶振。PCLK使用外部晶振贴了32M的U17。目前913A有输出如图所示。

         914A目前的贴片模式10bit.MODE贴是R1 11K OSS_SB OEN  SEL 这三个信号都是拉高。BISTEN直接拉到地。PDN是高电平。

        目前量取了PCLK输出没有信号,LOCK是低电平,0.57V..PASS电平是0.38V.

        ID的配置是40 R41都是0欧姆。I2C配置地址。0x60去读取,失败。

        想请教下,硬件是否有哪里没做好?