When using HSDCPro Automation DLL ADC Example, error code 1379 has been reported. I used HSDCPROV5.20, Labview 2014, and installed the runtime module. I tried to reinstall it, but it still hasn't solved the problem. Someone can help me answer or provide me with the download address of HSDC4.10.