This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3664EVM: ADC3664EVM

Part Number: ADC3664EVM


ADC3664EVM可以通过ADC35XX EVM GUI进行配置,我在配置的时候,对寄存器0x21写入值0xe0,然后重新读取0x21寄存器可以读到该值是0xe0.

在配置完成之后,将USB拔掉后重新接入,且重新打开ADC35XX EVM GUI,此时我再次读取寄存器0x21,发现该寄存器的值变成了0xfc(这是默认值,需要复位后才会出现,或者手动配置寄存器才行),在此以前我并没有进行硬件复位(按S1)或者软件复位。

请问:是不是ADC3664EVM每次上电,都需要先用ADC35XX EVM GUI进行配置成所需模式(如14 bit 1wire Bypass Mode (No Decimation)模式),且在调试板子的过程中不能关闭ADC35XX EVM GUI和给ADC3664EVM板子断电?否则,当板子重新上电的时候,ADC3664EVM将会自动变回默认运行状态(也即14 bit, 2W Bypass Mode (No Decimation) 模式)

 

  • 您好,每次断电再重启的话,寄存器的值都会恢复到默认值。

    那么关于GUI的话,GUI的配置在关闭之后,再打开是要重新配置的。

    如果GUI对寄存器的配置已经加载到芯片里了,只要芯片不断电,不复位,寄存器的值是应该不会恢复到默认值的。