This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1115: 测量电压不稳定,请问如何精准控制需要测量的信号的电平脉宽

Part Number: ADS1115

我使用FPGA将信号输出,将此信号经过一个NMOS管后接入ADS1115进行单端测量,目标点的电压为2.5v,ADC的寄存器设置部分FSR:4.096v,不使用比较器,采样率为860SPS;

1.我需要做的是在每个采样时间内精准打开NMOS管以精准测量打开时的电压,没法去做精准控制?

2.还有就是为什么使用单次转换模式一直不起作用?只能使用连续模式才有作用

3.请问我该如何去做,或者说有关于ADS1115的这部分资料有吗,

I2C详细寄存器配置如下:写:(10010000,00000001,11000010,11100011)

                                         读:(10010000,00000000,10010001