This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: OE是否需要下拉问题

Part Number: TXS0102


目前我的TXS0102设计如下,OE是通过10K电阻上拉到VCCA的电源

但是手册有描述要求在VCCA和VCCB上电前,OE需要保持低电平。

麻烦问下

1、我现在这样设计是否会有问题

2、在VCCA和VCCB上电完成前,为什么OE需要保持低电平

  • 您好, 已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 感谢您对TI产品的关注!
    关于你的咨询,你这样设计,OE是通过10K电阻上拉到VCCA的电源是没问题的。
    1和2问,你可以看看下面的说明。

    The datasheet says:ensure the high-impedance state during power up or power down, OE should be tied to GND through a pulldown resistor.

    If you do not care about the state of the I/O pins during power up/down, you can connect it to VCC.
    external pullups at the I/Os can also be removed as the device has internal 10kohm pullups already. Current implementation will lead to higher VOL levels.

    www.ti.com.cn/.../scea060.pdf