• ADS1274: adc电压输入范围和采集波形出现异常

    Part Number: ADS1274

    1、基准电压2.5v,AINN输入2.5v直流恒定电压,AINP摆动范围在0~5v,当AINP输入直流电压为2.5+1.25=3.7v左右 ,adc输出数据为68c521已经接近7FFFFF,电压加到4v左右出现输出出现负值,非7FFFFF

    不应该时AINP输入电压为5v时才会满量程7FFFFF吗?还有就是电压超过量程后应该是一直输出7FFFFF,实际却是负值?

    2、采集波形异常,下图1是示波器测量AINP处的信号波形,图2是ADC实际采集到的波形,发生…

  • ADS1274: Using the ready pin of the ADS1274 as an interrupt to run the spi acquisition program will get stuck at the read/write register

    Part Number: ADS1274

    The controller platform is ZYNQ7010.
    Use zynq's spi function interface to poll read/write data from the ADS1274. When I want to use the ready pin interrupt to read and write AD data, the program will get stuck in the read and write…

  • ADS1274: ADS1274 对应的verilog demo能提供吗?如果官方提供的话能给出对应网址吗?

    Part Number: ADS1274

    ADS1274 对应的verilog demo能提供吗?如果官方提供的话能给出对应网址吗?

  • ADS1274: 差分adc量程是正负2.5v,负电压为补码输出,是如何测量得出的?

    Part Number: ADS1274

    上图为adc测量流程图,采样电容为9PF,采样完是如何量化的?当VIN+电压小于VIN-电压,为什么可以测出是负值?不太明白

  • ADS1274: ADS1274数据手册中CLK/SCLK的频率比为1,2,4,8,其他比值可以吗?

    Part Number: ADS1274

    在ADS1274的datasheet中30页中有如下描述:“For best performance, limit fsclk/fclk to ratios of 1, 1/2,1/4,1/8, etc.”

    请问:fsclk/fclk 的比值能是其它值吗? 如果不是数据手册中的1,1/2,1/4,1/8 而是其他值,ads1274 芯片会正常运行吗?会有什么坏的结果吗?

  • ADS1274: IN+接单端信号输入,信号是以2.5v为直流基准,交流摆动范围为0-5v,请问IN-端可以接2.5v来实现±VREF采集范围吗?还是应该接GND实现0-2.5v范围

    Part Number: ADS1274

    hi,我现在正在使用ADS1274,这是一款差分输入ADC,IN+接单端信号输入,信号是以2.5v为直流基准,交流摆动范围为0-5v,请问IN-端可以接2.5v来实现±VREF采集范围吗?还是应该接GND实现0-2.5v范围

  • AD前端放大电路

    Other Parts Discussed in Thread: ADS1274, OPA350, OPA2277, OPA227, ADS1256, THS4521, OPA2209

    各位专家, 最近使用ADS1274采集小信号,基准电压电路参照开发板电路,REF5025+OPA350;

    输入设计为全差分输入,调试时使用开关电源作为输入源,伪差分输入,AINP1接电源+(12mv),AINN1接电源-(地)。 

     AVDD=5v,AGND=0V。

    第一种情况:

    采集数据计算后11.800mv,有300uv左右跳变…

  • ads1274前端驱动器对精度的影响

    Other Parts Discussed in Thread: THS4521, OPA2277, OPA227, ADS1274, LP38798

    TI 各位专家

    最近项目作数据采集卡,采集传感器的模拟信号,信号小于20mv。

    采集卡的模拟部分使用1:1的THS4521+ADS1274组成,差分信号输入,基本上照搬ADS1274数据手册上推荐的电路,应用正常,只是精度较低为16位。

    目前希望提高采集精度,想请教一下,下面方法是否能提高采集精度:

    牺牲输入的动态范围,规定输入的模拟信号<20mv…

  • ads1274前端放大

    Other Parts Discussed in Thread: ADS1274, OPA2277, OPA2350, THS4521, LP38798

    使用Ads1274 采集传感器信号,输入信号小于20mv,阻抗390欧姆。

    基本思路是将输入信号放大125倍,小于2.5V,满足ADS1274输入范围,希望能提高精度。

    前端放大电路由OPA2277+THS4521构成仪表放大电路后接入AD芯片,基准电压用Ref5025+OPA2350,具体如上图示。

    现在测试遇到问题:

    1.125倍放大时,输入信号6mv时…

  • ADS1274采样率疑问

    Other Parts Discussed in Thread: ADS1274

    我们用c6748的mcasp口驱动ADS1274,模式使用TDM,帧同步,高精度模式,但是采集的数据噪声非常大

    10分频HCLk频率为2.4Mhz,8分频fsclk 为300Khz,传输4个通道共96bit,则帧速率是300Khz/96=3125hz。

    按照datasheet说的,fdata=fHCLk/512=4687.5Hz, 现在传输速度是3125Hz,请问这种速率正确么?

      fdata=fFSYN=fsclk…

  • ads1274有丢码现象

    Other Parts Discussed in Thread: ADS1274

    我最近用了ads1274做压力传感器采样,用了两路,高精度模式,基于SPI的discrete模式,clk为5MHz,sclk为2.5MHz,SPS试过1k,500Hz,发现数据有丢码,很频繁,丢码后的数据接近于零电压输入,我输入了1hz正弦波,发现丢码后的数据接近于零输入,且组成了一个与输入正弦波同频的正弦波,只是幅值减小了一个比例,不知各位专家有过类似情况吗?不知是否我的采样率过高了?TI的专家能回答吗?非常谢谢!

  • ADS1274使用SPI读取的问题

    Other Parts Discussed in Thread: ADS1274

    请教各位,我用ADS1274的SPI方式读取,ADS1274使用高分辨率模式,数据输出为TDM动态方式,4通道全开启。SCLK/FCLK = 1,MCU的SPI的SCLK空闲状态为低电平,采用8位帧结构。

    MCU采用外部中断来接收DRDY下降沿信号,当DRDY信号下降沿来时进入中断,进入中断后先等待1个tclk,即上图中“tDS”,然后开启SPI,SPI每接收到1个字节就产生接收中断,接收中断将读到的这1个字节赋值到一个数组中…

  • ADS1274EVM无法正常下载固件

    Other Parts Discussed in Thread: ADS1274

    各位,

            刚刚买了一个ADS1274评估板,驱动都安装好了,但是PC连接评估板之后,却无法正常下载firmware,报错结果如下,不知道是什么问题,麻烦有经验的解答一下,谢谢了

  • ADS1274+THS4521的输入电压问题

    Other Parts Discussed in Thread: THS4521, ADS1274, ADS7813

    求教TI工程师,我用ADS1274+THS4521做采集,采用下图所示电路:

    在没有接入任何模拟输入信号的情况下,测量THS4521输入端VIN+与地之间的电压为2.5V,VIN-与地之间的电压也为2.5V,输出端AINN1和AINP1之间的差分电压为0V,请问这是正常的吗?

  • ads127

    Other Parts Discussed in Thread: ADS1274

    本人菜鸟新手一枚,在使用TI 的ADS1274时遇到一个问题。TI官方给出的ADS1274典型电路中,模拟地和数字地是分开连接的。但是看有的书(比如“运算放大器权威指南”)上说,AD芯片的数字地和模拟地需要全部接到模拟地上。那么请问对于ADS1274而言,到底“模拟地”和“数字地”是接在一起,还是分开连接,性能更好呢。尤其是对于电路噪声这一性能来说。…

  • ADS1274坏了,无DRDY信号输出

    Other Parts Discussed in Thread: ADS1274, THS4521, OPA1632, OPA2188, INA188

    ADS1274有CLK信号,但是没有DRDY信号输出,是否意味着芯片已经损坏?

    芯片工作正常应该一直有DRDY信号输出的,之前芯片一直是正常的,接了个传感器加载测试结果DRDY就没输出了,传感器输出应该没有超过1274的输入电压范围,即使超过,电路中也使用了限压二极管保护,换了一块1274再试,在空载的时候工作正常,加载后开始正常,后来又出现这种现象…

  • ADS1274的模拟电源和数字电源可以使用隔离电源分别供电吗?不共地

    Other Parts Discussed in Thread: ADS1274

    请问ADS1274的模拟电源AVDD to AGND与模拟电源DVDD,IOVDD to DGND可以使用隔离电源分别单独供电吗?两个电源不共地

  • ads1274上电顺序

    Other Parts Discussed in Thread: ADS1274

    ads1274的上电顺序,

    1、ADS1274的端口只供电,其他接口不接。我用tps70451,通过使能端,先给ads1274的DVDD供1.8v,然后IOVDD供3.3v,最后用tps7a3700,通过使能端,给ads1274的AVDD供5v电压。测量ads1274的VCOM端无电压输出;为啥?

    2、ADS1274的端口只供电,其他接口不接。我用tps70451,通过使能端,先给ads1274的DVDD供1.8v,但是IOVDD不提供3…

  • ads1274上电问题

    Other Parts Discussed in Thread: ADS1274

    ads1274的上电顺序,

    1、ADS1274的端口只供电,其他接口不接。我用tps70451,通过使能端,先给ads1274的DVDD供1.8v,然后IOVDD供3.3v,最后用tps7a3700,通过使能端,给ads1274的AVDD供5v电压。测量ads1274的VCOM端无电压输出;为啥?

    2、ADS1274的端口只供电,其他接口不接。我用tps70451,通过使能端,先给ads1274的DVDD供1.8v,但是IOVDD不提供3…

  • ADS1274和ADS1234的区别

    Other Parts Discussed in Thread: ADS1274, ADS1234

    请问TI的ADS1274和ADS1234的区别是什么?

    1. 好像ADS1234最大增益128,不知道在最大增益128的情况下,前段的桥式压力信号还能否继续放大后作为输入信号?

    2. 另外如果对于采样率不很敏感的话是否两个是一样的了,ADS1274比较高级是不是就是采样率比较高啊?

    3. 是不是可以这样说:如果用在衡器上,ADS1234适合静态称重,ADS1274适合动态称重?

    谢谢!

  • ADS1274 24位精度与参考电压的关系

    Other Parts Discussed in Thread: ADS1274

             请问ADS1274在使用16位时,参考电压为2.5V,1mV是否代表32767/2500=13 个数,如果参考电压不变的情况下,提高至17位数,相应的噪声也会随之增加。但是,如果提高至17位位数的同时,参考电压提高至3V,是否会好一点呢?是不是参考电压和ADC的位数有一定的关系呢?

  • ADS1274+THS4521 能否采集更宽的电压范围

    Other Parts Discussed in Thread: THS4521, ADS1274

    目前使用ADS1274+THS4521做压力方面的应用,2.5V的ommon-mode input voltage (VCM),实际测试时发现,我们1mV的压力代表十几个内码数。

    A   请问ADS1274是否最大就支持2.5V的ommon-mode input voltage (VCM)的,如果能支持更大的话,我们可以让1mV的压力代表的内码数值降低,相应的精度会提高。

    B   请问,如果ADS1274…

  • ADS1274 ESD 问题

    Other Parts Discussed in Thread: ADS1274

    TI工程师,您好

            目前我司购买的ADS1274经常被静电打坏,后面去做静电测试,ADS1274很容易被打坏,现象有两种:1.   ADS直接坏掉,SCLK有clock,但DRDY引脚没有数据。  2.  用电流表测试,芯片电流突然从0.1A增大到1A以上,如果断电及时,再次开机还可以使用,如果断电不及时,芯片会被烧掉。

            我感觉100多元的一个芯片的ESD能力应该不会有问题吧。     

            请帮忙分析是不是我们电路那个地方有需要改善啊…

  • ADS1274采样数据波动太大问题

    Other Parts Discussed in Thread: ADS1274, ADS1174

    TI工程师,您好!

          我司产品用到ADS1274芯片,参考电压2.5V,模式为高精度,FCLK为500K,采样率大概为1K,测量我们的差分信号电压及参考电压波动不超过200uV,使用16位的数据格式输出。

    1.  按照参考电压2.5V,16位的数据输出格式,1mv的电压应该大概代表26个数据,但是我们采集100个数值的最大最小值差距60,每100个数据进行平均求值,10秒内数值波动在10个数左右。

  • 关于ADS1274,转换所得数据噪声很大,毛刺多?

    自己设计了个AD转换的电路,结果转换所得结果噪声很大,下面是测得的信号数据绘制的曲线,请给分析一下。 真实的曲线应该和其包络线差不多。

1 2 3 4 5 »