This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
好。我司新项目使用的是新DMD: DLP3010LC
做板子参考的是TI官方的demo:TIDA-080003_DLP3010EVM-LC_DisplayBoard_SCH_RevB,使用的是DLPC3478+DLP3010+DLPA2005。未使用MSP430,只增加了CY7C65215与官方GUI进行通信控制。
目前状态:DLPC3478的SPI FLASH固件可以正学烧写,但是一直显示Power Off。发现DLPC3478的HOST_IRQ信号上电后一直为高,没有拉低。根据datasheet说明,如果HOST_IRQ没有拉低,那么不能进行I2C通信。但是怎么才能使其拉低呢?造成其一直为高的原因是什么才导致初使化不成功?
注:没有连接DMD,因为DMD的连接板还没有回来,要到十一后才可以回来。可能是因为没有连接DMD而导致DLPC3478初使化不成功吗?这样导致HOUST_IRQ一直为高?
期待您的回复。
您好!
请问DMD的型号是什么?DLP3010A还是DLP3010LC或者是DLP3010?
HOST_IRQ一直为高吗?还是会有一个负脉冲?
Best regards