This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3478的HOST_IRQ信号上电后一直为高无法初使化

Other Parts Discussed in Thread: DLP3010LC, DLP3010EVM-LC, DLP3010, DLPC3478, DLPA2005, TIDA-080003

好。我司新项目使用的是新DMD: DLP3010LC
做板子参考的是TI官方的demo:TIDA-080003_DLP3010EVM-LC_DisplayBoard_SCH_RevB,使用的是DLPC3478+DLP3010+DLPA2005。未使用MSP430,只增加了CY7C65215与官方GUI进行通信控制。
目前状态:DLPC3478的SPI FLASH固件可以正学烧写,但是一直显示Power Off。发现DLPC3478的HOST_IRQ信号上电后一直为高,没有拉低。根据datasheet说明,如果HOST_IRQ没有拉低,那么不能进行I2C通信。但是怎么才能使其拉低呢?造成其一直为高的原因是什么才导致初使化不成功?
注:没有连接DMD,因为DMD的连接板还没有回来,要到十一后才可以回来。可能是因为没有连接DMD而导致DLPC3478初使化不成功吗?这样导致HOUST_IRQ一直为高?
期待您的回复。

x 出现错误。请重试或与管理员联系。