订单RKPMB7-2403270002 项次120,130,140 同时做了3行交期变更,2行成功了,其中一行报这样的错误。请问是因为传的一次传的变更数据太多导致的,还是因为其他原因导致的
Order is in process by another application and cannot accept changes at this time. Wait 5 minutes before attempting to resubmit your request. If issue continues, contact TI customer support
单独发送不会报错,但是我们存在很多批量变更交期的情况。如果我们把同一个订单所有的变更行放在一个变更文件里面一次发送给TI,是否就可以避免一次传太多行导致的这个报错。
我建议你可以将同一个PO的多行改动放在一个API PO Change transaction 中,但是尽量也不要一次超过15个item否则API response的时间也会相对较长.
可以的,不过process time会久一点,可能最长会需要4到5分钟左右。
你可以试试应该是可行的,你们的order change是每天都需要高频次的改动么?
刚试了一下间隔5s发送,部分订单行还是无法更改成功。能否帮忙查一下,失败的真正原因。订单:RKPMB7-2403270002 更改时间在16:26分以后更改了CRD
我这边看今天发送的都是没问题的,只有昨天的一笔是429 报错你看是下面这个error 么?
昨天收到了很多笔拒绝提示:Order is in process by another application and cannot accept changes at this time. Wait 5 minutes before attempting to resubmit your request. If issue continues, contact TI customer support
没有收到TI-API-0429 这个报错,TI-API-0429 是指我们变更的次数太多了吗