订单RKPMB7-2403270002 项次120,130,140 同时做了3行交期变更,2行成功了,其中一行报这样的错误。请问是因为传的一次传的变更数据太多导致的,还是因为其他原因导致的
Order is in process by another application and cannot accept changes at this time. Wait 5 minutes before attempting to resubmit your request. If issue continues, contact TI customer support
我建议你可以将同一个PO的多行改动放在一个API PO Change transaction 中,但是尽量也不要一次超过15个item否则API response的时间也会相对较长.
可以的,不过process time会久一点,可能最长会需要4到5分钟左右。
你可以试试应该是可行的,你们的order change是每天都需要高频次的改动么?
刚试了一下间隔5s发送,部分订单行还是无法更改成功。能否帮忙查一下,失败的真正原因。订单:RKPMB7-2403270002 更改时间在16:26分以后更改了CRD
我这边看今天发送的都是没问题的,只有昨天的一笔是429 报错你看是下面这个error 么?
昨天收到了很多笔拒绝提示:Order is in process by another application and cannot accept changes at this time. Wait 5 minutes before attempting to resubmit your request. If issue continues, contact TI customer support
没有收到TI-API-0429 这个报错,TI-API-0429 是指我们变更的次数太多了吗