使用场景:温湿度监测系统1根485总线上有4~25个相同的监测终端从机节点,总线最长600米,通讯速率为9600~115200。(每个节点的MCU是STM32G070,引脚耐压5V,485芯片是THVD1500,每个节点功耗约70mW/h,瞬间最大电流小于150mA),主机是12V工控电脑的232或USB转THVD1500的(电脑功率为9W/h,瞬间最大电流小于3A),所有节点和电脑主机均使用12V电源统一供电,每个节点上均有4.2V锂电池,电池BAT转3.3V给MCU,转5V给THVD1500,各个节点PCB中GND都是共地的,所有节点的GND用铜钱相连接,系统无连接其他大电流设备。允许忽略节点从机在开机上电瞬间时的信号干扰,只要保证正常工作时无信号干扰即可,正常工作时,主机每分钟会定时广播一条指令,每个节点会按ID号顺序上传12字节的数据,每个节点上传间隔会保持6ms空闲,请问这样的应用每个节点上MCU的USART_TX、RX到THVD1500有必要添加数字隔离器吗?我感觉总线所有节点都是共地的,也无接入大电流设备,添加隔离器的意义不大,如果必须添加数字隔离器,请问选择默认为高电平的还是选择默认为低电平的合适呢?