TCAN4550-Q1: 加载完驱动之后,中断计数一直在增加,直到系统禁用该中断

Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550

我们使用的是NVIDIA Jetson Thor平台,通过SPI拓展CAN,具体电路如下:

image.png

VSUP已经链接到了12V,并将R9电阻取消焊接,

使用的驱动代码是:

m_can - drivers/net/can/m_can - Linux source code (v6.8.12) - Bootlin Elixir Cross Referencer

设备树配置如下:

spi@810c590000 {
                        status = "okay";
                        spi@0 {
                                status = "okay";
                                compatible = "ti,tcan4x5x";
                                reg = <0x0>;
                                #address-cells = <1>;
                                #size-cells = <1>;
                                spi-max-frequency = <10000000>;
                                bosch,mram-cfg = <0x0 0 0 16 0 0 1 1>;
                                clocks = <&tcan4x5x_clk>, <&tcan4x5x_clk>;
                                clock-names = "hclk", "cclk";
                                interrupt-parent = <&gpio_aon>;
                                interrupts = <TEGRA264_AON_GPIO(DD, 4) IRQ_TYPE_LEVEL_LOW>;
                                //device-state-gpios = <&gpio3 21 GPIO_ACTIVE_HIGH>;
                                //device-wake-gpios = <&gpio1 15 GPIO_ACTIVE_HIGH>;
                                reset-gpios = <&gpio_aon TEGRA264_AON_GPIO(DD, 3) GPIO_ACTIVE_HIGH>;
                                controller-data {
                                        nvidia,enable-hw-based-cs;
                                        nvidia,rx-clk-tap-delay = <0x10>;
                                        nvidia,tx-clk-tap-delay = <0x0>;
                                };
                        };

加载驱动之后的日志如下:

[  109.198684] irq: IRQ398: trimming hierarchy from :bus@0:pmc@c800000
[  109.201510] tcan4x5x spi0.0: Detected TCAN device version generic
[  109.201669] tcan4x5x spi0.0: ----plink----tcan4x5x_clear_interrupts ----
[  109.203484] tcan4x5x spi0.0: ----plink----tcan4x5x_clear_interrupts ----
[  109.204219] tcan4x5x spi0.0: m_can device registered (irq=398, version=32)
[  109.204225] tcan4x5x spi0.0 can4: TCAN4X5X successfully initialized.

 

操作如下:

nvidia@tegra-ubuntu:~$ sudo modprobe can
[sudo] password for nvidia:
nvidia@tegra-ubuntu:~$ sudo modprobe can-raw
nvidia@tegra-ubuntu:~$ sudo insmod m_can.ko
nvidia@tegra-ubuntu:~$ sudo insmod tcan4x5x.ko
nvidia@tegra-ubuntu:~$ sudo ip link set can4 type can bitrate 500000
nvidia@tegra-ubuntu:~$ sudo ip link set up can4
nvidia@tegra-ubuntu:~$ sudo ip link set down can4

 

当通过IP link打开can总线之后,dmesg日志会一直输出下述内容:

[  155.365846] ----plink---- m_can_open ----
[  155.383143] tcan4x5x spi0.0: ----plink----tcan4x5x_clear_interrupts ----
[  157.480670] tcan4x5x spi0.0: ECR=0x00000000 (TEC=0, REC=0)
[  157.480683] ----plink---- m_can_isr ----
[  157.480687] tcan4x5x spi0.0: ----plink---- m_can_interrupt_handler ----
[  157.480787] tcan4x5x spi0.0: ----plink----tcan4x5x_clear_interrupts ----
[  157.481023] tcan4x5x spi0.0: ISR triggered: IR=0x00000000 PSR=0x0000070f

[  159.578596] tcan4x5x spi0.0: ECR=0x00000000 (TEC=0, REC=0)
[  159.578608] ----plink---- m_can_isr ----
[  159.578612] tcan4x5x spi0.0: ----plink---- m_can_interrupt_handler ----
[  159.578721] tcan4x5x spi0.0: ----plink----tcan4x5x_clear_interrupts ----
[  159.578965] tcan4x5x spi0.0: ISR triggered: IR=0x00000000 PSR=0x0000070f

[  161.675261] tcan4x5x spi0.0: ECR=0x00000000 (TEC=0, REC=0)
[  161.675273] ----plink---- m_can_isr ----
[  161.675276] tcan4x5x spi0.0: ----plink---- m_can_interrupt_handler ----
[  161.675707] tcan4x5x spi0.0: ----plink----tcan4x5x_clear_interrupts ----
[  161.676621] tcan4x5x spi0.0: ISR triggered: IR=0x00000000 PSR=0x0000070f

[  163.773759] tcan4x5x spi0.0: ECR=0x00000000 (TEC=0, REC=0)
[  163.773780] ----plink---- m_can_isr ----
[  163.773787] tcan4x5x spi0.0: ----plink---- m_can_interrupt_handler ----
[  163.774490] tcan4x5x spi0.0: ----plink----tcan4x5x_clear_interrupts ----
[  163.775033] tcan4x5x spi0.0: ISR triggered: IR=0x00000000 PSR=0x0000070f
[  165.870509] tcan4x5x spi0.0: ECR=0x00000000 (TEC=0, REC=0)
[  165.870534] ----plink---- m_can_isr ----
[  165.870541] tcan4x5x spi0.0: ----plink---- m_can_interrupt_handler ----
[  165.871268] tcan4x5x spi0.0: ----plink----tcan4x5x_clear_interrupts ----
[  165.871837] tcan4x5x spi0.0: ISR triggered: IR=0x00000000 PSR=0x0000070f

 

同时中断计数会一直增加,直到关闭CAN总线

现象如下:

nvidia@tegra-ubuntu:~$ sudo ip link set up can4
nvidia@tegra-ubuntu:~$ cat /proc/interrupts |grep 398
398:         11          0          0          0          0          0          0          0          0          0          0          0          0          0 cf00000.gpio  22 Level     can4
nvidia@tegra-ubuntu:~$ cat /proc/interrupts |grep 398
398:         11          0          0          0          0          0          0          0          0          0          0          0          0          0 cf00000.gpio  22 Level     can4
nvidia@tegra-ubuntu:~$ cat /proc/interrupts |grep 398
398:         12          0          0          0          0          0          0          0          0          0          0          0          0          0 cf00000.gpio  22 Level     can4
IPI1:     14863      17983      14218      21255      12577      19493      48290      13692      14282      20918      16944      15354      53524      23989       Function call interrupts
nvidia@tegra-ubuntu:~$ cat /proc/interrupts |grep 398
398:         13          0          0          0          0          0          0          0          0          0          0          0          0          0 cf00000.gpio  22 Level     can4
nvidia@tegra-ubuntu:~$ cat /proc/interrupts |grep 398
398:         14          0          0          0          0          0          0          0          0          0          0          0          0          0 cf00000.gpio  22 Level     can4
nvidia@tegra-ubuntu:~$ cat /proc/interrupts |grep 398
398:         15          0          0          0          0          0          0          0          0          0          0          0          0          0 cf00000.gpio  22 Level     can4
nvidia@tegra-ubuntu:~$ cat /proc/interrupts |grep 398
398:         15          0          0          0          0          0          0          0          0          0          0          0          0          0 cf00000.gpio  22 Level     can4
nvidia@tegra-ubuntu:~$ sudo ip link set down can4

 

这个情况会持续到系统自动禁用该中断,并且系统日志输出如下内容:

[ 5620.598322] irq 398: nobody cared (try booting with the "irqpoll" option)
[ 5620.598375] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G           OE      6.8.12-1021-tegra #1
[ 5620.598383] Hardware name: NVIDIA NVIDIA Jetson AGX Thor Developer Kit/Jetson, BIOS 39.2.0-gcid-45755727 06/01/2026
[ 5620.598389] Call trace:
[ 5620.598393]  dump_backtrace+0x90/0xf0
[ 5620.598413]  show_stack+0x18/0x2c
[ 5620.598418]  dump_stack_lvl+0x7c/0x9c
[ 5620.598442]  dump_stack+0x18/0x2c
[ 5620.598449]  __report_bad_irq+0x38/0xe8
[ 5620.598460]  note_interrupt+0x320/0x370
[ 5620.598464]  handle_irq_event+0xa4/0xb8
[ 5620.598486]  handle_level_irq+0xc0/0x1a8
[ 5620.598494]  handle_irq_desc+0x48/0x80
[ 5620.598500]  generic_handle_domain_irq+0x1c/0x30
[ 5620.598508]  tegra186_gpio_irq+0x138/0x280
[ 5620.598525]  handle_irq_desc+0x48/0x80
[ 5620.598530]  generic_handle_domain_irq+0x1c/0x30
[ 5620.598537]  gic_handle_irq+0x4c/0x12c
[ 5620.598543]  call_on_irq_stack+0x30/0x48
[ 5620.598551]  do_interrupt_handler+0x88/0x9c
[ 5620.598558]  el1_interrupt+0x34/0x70
[ 5620.598567]  el1h_64_irq_handler+0x18/0x2c
[ 5620.598573]  el1h_64_irq+0x68/0x6c
[ 5620.598576]  cpuidle_enter_state+0xc0/0x4c4
[ 5620.598583]  cpuidle_enter+0x38/0x58
[ 5620.598596]  do_idle+0x1fc/0x278
[ 5620.598605]  cpu_startup_entry+0x34/0x3c
[ 5620.598611]  kernel_init+0x0/0x1ec
[ 5620.598616]  arch_post_acpi_subsys_init+0x0/0x18
[ 5620.598631]  start_kernel+0x54c/0x6f4
[ 5620.598636]  __primary_switched+0xb8/0xc0
[ 5620.598646] handlers:
[ 5620.598659] [<00000000e3ce55da>] irq_default_primary_handler threaded [<00000000e676cd34>] m_can_class_suspend [m_can]
[ 5620.604031] Disabling IRQ #398

 

中断被禁用之后将无法再接受或者发送CAN数据

 

使用的内核版本如下:

nvidia@tegra-ubuntu:~$ uname -a
Linux tegra-ubuntu 6.8.12-1021-tegra #1 SMP PREEMPT Mon Jun  1 13:25:46 PDT 2026 aarch64 aarch64 aarch64 GNU/Linux

 

请问有什么好的解决方案嘛?

 

  • 当总线UP之后,我通过示波器查看到,终端引脚在中断计数增加的时候,周期性的被拉低

  • 当总线UP之后,我通过示波器查看到,终端引脚在中断计数增加的时候,周期性的被拉低

  • 您好

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 我专精于TCAN4550-Q1器件,而非Linux系统。我不确定如何解读您分享的Linux日志文件截图。日志中显示错误计数器、中断寄存器和协议状态寄存器(ECR、IR和PSR)的部分,并未提供任何关于哪些中断位被置位的信息,也没有显示任何错误。

    TCAN4550-Q1 通常需要发送错误计数器 (TEC) 超过最大值才能断开与 CAN 总线的连接,从而进入总线关闭状态。最常见的原因是标称位或数据位时序配置存在问题,或者存在时钟容差问题。

    请验证标称位和数据位时序是否与网络上的所有其他设备匹配,以及时钟频率是否在 ISO 11898-1 标准要求的容差范围内。

    问候,

    乔纳森

  • 有关于TCAN4550器件时钟要求的详细说明嘛?当前的情况CAN总线能正常收发,但是在空闲状态频繁的触发中断,这不符合实际的应用。

    另外,TCAN4550的驱动程序,我是直接从内核中获取的源码进行编译的。从源码中的信息来看,驱动程序是你们提供的Dan Murphy <dmurphy@ti.com>

    能否申请一位同时了解Linux系统的支持呢?目前这个问题已经困惑我们很久了。希望得到你们的帮组

  • 请问您有TCAN4550器件时钟要求的详细说明吗?目前,CAN总线可以正常收发数据,但在空闲状态下频繁触发中断,这不适用于实际应用。

    您能告诉我空闲状态下具体生成了哪些中断位吗?如果可以,我可以帮助您理解这些位被置位的原因,并帮助您确定如何阻止它们被置位。请告诉我寄存器 0x​​000C、0x0820 和 0x0824 的值,以便我查看哪些状态位和中断位被置位。

    我们有几份应用报告讨论了时钟电路的优化要求,尤其是在使用晶振时。使用单端时钟通常不是问题,时钟信号只需是符合数据手册要求的单端信号即可。

    TCAN455x 时钟优化和设计指南应用报告链接

    TCAN455x-Q1 外围电路和时钟设计应用报告链接

    如果您的问题更侧重于 CAN 通信的时钟要求,那么 ISO 11898-1 标准以及许多其他文档中都列出了一些要求,这些文档讨论了如何分配时间量子以获得良好的采样点。TCAN4550-Q1 使用了博世开发的 MCAN IP,有一篇应用笔记详细讨论了 CAN FD 位定时配置,您可能对此感兴趣。

    CAN FD链路)的比特时间要求

    ISO 11898-1 时钟振荡器容差规范要求如下:

    MCAN 控制器有一份由博世为其知识产权编写的用户手册,其中可能还包含其他您感兴趣的详细信息。

    MCAN 用户手册链接

    此外,我直接从内核源代码编译了 TCAN4550 驱动程序。根据源代码中的信息,该驱动程序由Dan Murphy <dmurphy@ti.com> 提供。

    是的,没错。该驱动程序最初由 Dan Murphy 开发,并在 Linux 内核 5.14 版本中合并到上游。后来,在 2020 年由第三方开发者进行了更新。您提供的链接包含的是更新后的版本。

    能否请一位精通 Linux 系统的人员提供帮助?这个问题困扰我们很久了。非常感谢您的帮助。

    如果你的问题出在 Linux 代码上,那么你需要向 Linux 社区寻求帮助,因为该驱动程序已经合并到内核中了。

    如果您遇到的问题与设备运行正常或设备错误有关,例如硬件或应用程序中的寄存器配置问题,那么我是该设备的专家,可以为您解答这些问题。但是,我对数据日志及其格式并不熟悉,如果其中包含调试问题所需的详细设备寄存器值,我就不清楚了。以下日志中似乎没有设置任何错误计数器位、中断位或协议状态信息,因此我不清楚问题出在哪里。

    请解释如何解读以下日志。各列和数字分别代表什么?

    请解释一下如何解读另一份日志。

    但如果你能直接与我沟通 TCAN4550 设备的寄存器值,那就更好了。

    问候,

    乔纳森

  • 我无法在论坛上直接恢复消息了,只能以邮件的方式发送给你,同时在之前的消息上进一步进行回复。
    其实我们现在不确定具体是驱动的问题,还是由于硬件电路上时钟的问题,所以需要你们的协助。
    关于芯片的寄存器值如下,我导出了所有的寄存器的值
    [ 4100.554333] tcan4x5x spi0.0: ===== TCAN4x5x Register Dump after init =====
    [ 4100.554336] tcan4x5x spi0.0: --- Device ID and SPI Registers ---
    [ 4100.554680] tcan4x5x spi0.0: DEV_ID1 (0x0000): 0x4e414354
    [ 4100.555034] tcan4x5x spi0.0: DEV_ID2 (0x0004): 0x30353534
    [ 4100.555093] tcan4x5x spi0.0: REV (0x0008): 0x00110201
    [ 4100.555441] tcan4x5x spi0.0: STATUS (0x000c): 0x00000008
    [ 4100.555793] tcan4x5x spi0.0: ERROR_STATUS_MASK (0x0010): 0x3f3f0000
    [ 4100.555797] tcan4x5x spi0.0: --- Device Config and Interrupt Registers ---
    [ 4100.555852] tcan4x5x spi0.0: CONFIG (0x0800): 0x080004a8
    [ 4100.556249] tcan4x5x spi0.0: TS_PRESCALE (0x0804): 0x00000002
    [ 4100.556582] tcan4x5x spi0.0: TEST_REG (0x0808): 0x00000000
    [ 4100.556918] tcan4x5x spi0.0: Test 2 (0x080c): 0x00000000
    [ 4100.557252] tcan4x5x spi0.0: INT_FLAGS (0x0820): 0x00000082
    [ 4100.557315] tcan4x5x spi0.0: MCAN_INT_REG (0x0824): 0x00010000
    [ 4100.557373] tcan4x5x spi0.0: INT_EN (0x0830): 0x8096a8ff
    [ 4100.557377] tcan4x5x spi0.0: --- M_CAN Key Registers ---
    [ 4100.557432] tcan4x5x spi0.0: CCCR (0x100c): 0x00000a33
    [ 4100.557487] tcan4x5x spi0.0: NBTP (0x1010): 0x00000080
    [ 4100.557542] tcan4x5x spi0.0: TSCONFIG (0x1014): 0x00000000
    [ 4100.557597] tcan4x5x spi0.0: TOCC (0x1018): 0x00000000
    [ 4100.557652] tcan4x5x spi0.0: ECR (0x1020): 0x000f0001
    [ 4100.557707] tcan4x5x spi0.0: PSR (0x1024): 0x000000cf
    [ 4100.557762] tcan4x5x spi0.0: TDCR (0x1028): 0xffff0000
    [ 4100.557816] tcan4x5x spi0.0: IE (0x1040): 0x00000000
    [ 4100.557870] tcan4x5x spi0.0: ILS (0x1044): 0x0000070f
    [ 4100.557926] tcan4x5x spi0.0: IR (0x1048): 0x00000000
    [ 4100.557982] tcan4x5x spi0.0: ILCR (0x104c): 0x00000000
    [ 4100.558048] tcan4x5x spi0.0: RXGFC (0x1050): 0x20010000
    [ 4100.558122] tcan4x5x spi0.0: XIDAM (0x1054): 0x07b79289
    [ 4100.558179] tcan4x5x spi0.0: HPMS (0x1058): 0x00000000
    [ 4100.558235] tcan4x5x spi0.0: NDAT1 (0x105c): 0x00000001
    [ 4100.558290] tcan4x5x spi0.0: NDAT2 (0x1060): 0x00000000
    [ 4100.558344] tcan4x5x spi0.0: RXFCS (0x1080): 0x00000000
    [ 4100.558400] tcan4x5x spi0.0: RXF0S (0x1084): 0x00000000
    [ 4100.558456] tcan4x5x spi0.0: RXFAP (0x1088): 0x00000000
    [ 4100.558513] tcan4x5x spi0.0: RXFS (0x1090): 0x1fffffff
    [ 4100.558569] tcan4x5x spi0.0: TXFQS (0x1098): 0x00000000
    [ 4100.558625] tcan4x5x spi0.0: TXEFA (0x109c): 0x00000000
    [ 4100.558683] tcan4x5x spi0.0: TXEFS (0x10a0): 0x00100000
    [ 4100.558739] tcan4x5x spi0.0: TXBTIE (0x10a8): 0x00000000
    [ 4100.558796] tcan4x5x spi0.0: TXBCIE (0x10ac): 0x00000000
    [ 4100.558852] tcan4x5x spi0.0: TXBIF (0x10b0): 0x00000480
    [ 4100.558908] tcan4x5x spi0.0: TXBCIE (0x10b4): 0x00000000
    [ 4100.558966] tcan4x5x spi0.0: TXBAR (0x10b8): 0x00000000
    [ 4100.559021] tcan4x5x spi0.0: TXBCR (0x10bc): 0x00000777
    [ 4100.559078] tcan4x5x spi0.0: TXBCS (0x10c0): 0x01000488
    [ 4100.559136] tcan4x5x spi0.0: TXEFA (0x10c8): 0x00000007
    [ 4100.559191] tcan4x5x spi0.0: CKDIV (0x10d0): 0x00000000
    [ 4100.559194] tcan4x5x spi0.0: ===== End Register Dump =====

    下图的日志中只需要关注我红框出来的一列,该数字表示中断触发的次数,正常情况下,只是将CAN总线打开,不进行数据的收发操作,中断次数不应该出现递增的情况。
    实际上无论是标准CAN还是CANFD都会出现这个问题,
    另外如果忽略这个问题直接进行收发测试的话,CAN或者CANFD都是正常的,只不过频繁增加的中断计数,会直接导致系统禁用掉该中断。从而导致CAN总线无法再进行数据的收发。
  • 你好,

    感谢您提供的补充信息,包括如何理解和解读您分享的信息以及提供的寄存器转储文件。但我注意到 MCAN 寄存器的名称或缩写与寄存器地址不匹配。

    根据提供的一些寄存器值,我认为名称有误,数据与日志中的地址关联。我已将日志中错误的名称用红色字体标出,并将正确的名称用蓝色字体标出。

    我还用蓝色字体标出了注册地址和名称,这样就能很清楚地看出蓝色名称与蓝色地址相关联。

    芯片的寄存器值如下;我已经导出了所有寄存器值。
    [4100.554333] tcan4x5x spi0.0: ===== 初始化后 TCAN4x5x 寄存器转储 =====
    [4100.554336] tcan4x5x spi0.0: --- 设备 ID 和 SPI 寄存器 ---
    [4100.554680] tcan4x5x spi0.0: DEV_ID1 ( 0x0000 ): 0x4e414354
    [4100.555034] tcan4x5x spi0.0: DEV_ID2 ( 0x0004 ): 0x30353534
    [4100.555093] tcan4x5x spi0.0: REV ( 0x0008 ): 0x00110201
    [4100.555441] tcan4x5x spi0.0:状态( 0x000c ): 0x00000008
    [4100.555793] tcan4x5x spi0.0: ERROR_STATUS_MASK ( 0x0010 ): 0x3f3f0000
    [4100.555797] tcan4x5x spi0.0: --- 设备配置和中断寄存器 ---
    [4100.555852] tcan4x5x spi0.0: CONFIG ( 0x0800 ): 0x080004a8
    [4100.556249] tcan4x5x spi0.0: TS_PRESCALE ( 0x0804 ): 0x00000002
    [4100.556582] tcan4x5x spi0.0: TEST_REG ( 0x0808 ): 0x00000000
    [4100.556918] tcan4x5x spi0.0:测试 2 ( 0x080c ): 0x00000000
    [4100.557252] tcan4x5x spi0.0: INT_FLAGS ( 0x0820 ): 0x00000082
    [4100.557315] tcan4x5x spi0.0: MCAN_INT_REG0x0824 ):0x00010000
    [4100.557373] tcan4x5x spi0.0: INT_EN ( 0x0830 ): 0x8096a8ff
    [4100.557377] tcan4x5x spi0.0: --- M_CAN 键寄存器 ---
    [4100.557432] tcan4x5x spi0.0: CCCR DBTP ( 0x100c ): 0x00000a33
    [4100.557487] tcan4x5x spi0.0: NBTP测试( 0x1010 ): 0x00000080
    [4100.557542] tcan4x5x spi0.0: TSCONFIG RWD ( 0x1014 ): 0x00000000
    [4100.557597] tcan4x5x spi0.0: TOCC CCCR0x1018 ):0x00000000
    [4100.557652] tcan4x5x spi0.0: ECR TSCC ( 0x1020 ): 0x000f0001
    [4100.557707] tcan4x5x spi0.0: PSR TSCV0x1024 ):0x000000cf
    [4100.557762] tcan4x5x spi0.0: TDCR TOCC0x1028 ):0xffff0000
    [4100.557816] tcan4x5x spi0.0: IE ECR ( 0x1040 ): 0x00000000
    [4100.557870] tcan4x5x spi0.0: ILS PSR ( 0x1044 ): 0x0000070f
    [4100.557926] tcan4x5x spi0.0:红外TDCR0x1048 ):0x00000000
    [4100.557982] tcan4x5x spi0.0: ILCR RSVD ( 0x104c ): 0x00000000
    [4100.558048] tcan4x5x spi0.0: RXGFC IR0x1050 ):0x20010000
    [4100.558122] tcan4x5x spi0.0: XIDAM IE ( 0x1054 ): 0x07b79289
    [4100.558179] tcan4x5x spi0.0: HPMS ILS0x1058 ):0x00000000
    [4100.558235] tcan4x5x spi0.0: NDAT1 ILE ( 0x105c ): 0x00000001
    [4100.558290] tcan4x5x spi0.0: NDAT2 RSVD ( 0x1060 ): 0x00000000
    [4100.558344] tcan4x5x spi0.0: RXFCS GFC ( 0x1080 ): 0x00000000
    [4100.558400] tcan4x5x spi0.0: RXF0S SIDFC ( 0x1084 ): 0x00000000
    [4100.558456] tcan4x5x spi0.0: RXFAP XIDFC ( 0x1088 ): 0x00000000
    [4100.558513] tcan4x5x spi0.0: RXFS XIDAM ( 0x1090 ): 0x1fffffff
    [4100.558569] tcan4x5x spi0.0: TXFQS NDAT1 ( 0x1098 ): 0x00000000
    [4100.558625] tcan4x5x spi0.0: TXEFA NDAT2 ( 0x109c ): 0x00000000
    [4100.558683] tcan4x5x spi0.0: TXEFS RXF0C ( 0x10a0 ): 0x00100000
    [4100.558739] tcan4x5x spi0.0: TXBTIE RXF0A ( 0x10a8 ): 0x00000000
    [4100.558796] tcan4x5x spi0.0: TXBCIE RXBC ( 0x10ac ): 0x00000000
    [4100.558852] tcan4x5x spi0.0: TXBIF RXF1C ( 0x10b0 ): 0x00000480
    [4100.558908] tcan4x5x spi0.0: TXBCIE RXF1S ( 0x10b4 ): 0x00000000
    [4100.558966] tcan4x5x spi0.0: TXBAR RXF1A ( 0x10b8 ): 0x00000000
    [4100.559021] tcan4x5x spi0.0: TXBCR RXESC ( 0x10bc ): 0x00000777
    [4100.559078] tcan4x5x spi0.0: TXBCS TXBC ( 0x10c0 ): 0x01000488
    [4100.559136] tcan4x5x spi0.0: TXEFA TXESC ( 0x10c8 ): 0x00000007
    [4100.559191] tcan4x5x spi0.0: CKDIV TXBAR ( 0x10d0 ): 0x00000000
    [4100.559194] tcan4x5x spi0.0: ===== 寄存器转储结束 =====
    看起来被置位的是时间戳回绕(TSW)计数器位。每次计数器达到最大值并回绕到计数器开头时,该中断位就会被置位。
    其原理是,如果系统需要跟踪 CAN 消息的接收时间,则可以使用这个时间戳计数器来记录消息。但是,一旦计数器循环回到起始位置,新接收到的消息的时间戳可能看起来比计数器计数较高时接收到的旧消息的时间戳更早。
    因此,每次计数器溢出时都会设置此中断位,以便MCU能够跟踪并正确处理时间戳日志,从而满足系统要求。但是,此计数器的值并不大,因此即使没有CAN通信,它也会周期性地产生中断。
    如果您不需要在时间戳计数器每次循环时都接收中断通知,可以通过将中断使能寄存器中的 TSWE 位设置为“0”来屏蔽或禁用它。(0x1054[16] = 0)
    您能否尝试一下这个方法,看看是否能解决您反复遇到的中断问题?
    问候,
    乔纳森