This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LMX2594相位噪声的问题



手册上标称相位噪声:归一化底噪为-236dBc/Hz,闪烁噪声为-129dBc/Hz,那么计算100MHz输入,200MHz鉴相,

输出15GHz时的相位噪声:底噪=-236+20log(1500/200)+10log(200*10^6)≈-115.5dBc/Hz;

                        100k处闪烁噪声=-129+20log(15)-10log(100/10)≈-115.5dBc/Hz;

那么在100KHz处的相位噪声应该为-112.5dBc/Hz@100kHz,但实际官方手册上给的实际测试见datasheet 上图6,在100KHz处只有-107.5(测试条件和以上计算相同),和理论计算相差5dB,作何解释?

另外,datasheet 上图4,100MHz鉴相频率下,输出12GHz时的相位噪声在100kHz处为-112dBc/Hz,但图8所示,200MHz鉴相频率下,实测输出11GHz时相位噪声在100kHz处为-109.4dBc/Hz,那么在100MHz鉴相时,相噪应增加3dB,为-106.4dBc/Hz,与输出12GHz的-112dBc/Hz折算出来也是相差5dB的。

请问官方作何解释?

我现在做了一个测试板,遇到两个问题。1、目前我测试的值和官方给的实测值有3dB差异,这个也有一定可能性,正在找问题。我用的恒温晶振相噪很好的,-158dBc/Hz@1kHz,-163dBc/Hz@10kHz,-168dBc/Hz@100kHz,输入功率也合适,不知道是不是单端输入或者正弦波的参考造成相噪差了3dB?目前正在查找问题。2、在输出7GHz时,VCO 14GHz除2得到,输出7GHz的同时,也输出3.5GHz和10.5HGz,3.5GHz约为-50dBc,10.5HGz约为-65dBc,难道7GHz又参与了分频?其实之前HIttite的可变分频器HMC862在低温时我们就遇到这种问题,不只有输入信号参与了分频!不知道官方有注意到以上问题没?

LMX2594相位噪声图.docx