This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们使用Broadcom的交换芯片(仅可使用固定千兆速率的sgmii协议)与DP83867通过4线的sgmii连接,DP83867外接RJ45引出。原理图参考评估板,可以从交换芯片侧看到该链路up上了,但是从DP83867这边的网口无法与交换芯片进行交互,已确认交换芯片工作正常。dp83867的寄存器信息如下:
地址 数据
0x01 7949
0x02 2000
0x03 A231
0x04 01E1
0x05 0000
0x06 0064
0x07 2001
0x08 0000
0x09 1300
0x0f 3000
0x10 5C48
0x11 A802
0x12 0000
0x13 0044
0x14 29C7
想问下这可能是什么原因,是我们对寄存器地址的配置有问题吗?
您好,loopback的测试我们今天做一下,我发现我们有个问题,就是虽然我们取消了AN模式设置了sgmii协议强制1000M速率,看寄存器值也是正确的,BMCR寄存器(地址0x0000)的值为0140,CFG2寄存器(地址0x0014)的值为写为2947,但是在读phy状态的时候只显示phy工作在10M的速率,是还有其他设置sgmii协议固定千兆速率的寄存器吗?
您好,我们今天又做了测试,发现把AN打开后即0x0000寄存器配为0140,把phy引出的RJ45接到千兆交换机上时phy以及交换机网口上的LED都处于正常绿灯闪烁,应该说明从千兆交换机侧看link已经建立了。当前应用环境如下:switch(仅支持固定千兆sgmii协议)——>phy——>RJ45——>千兆交换机。还是怀疑switch——>phy这边有问题,dp83867是否支持四线的sgmii固定千兆速率呢?目前看寄存器0x13的值为0044,说明是有xGMII相关错误的。
您好,您看下是否是寄存器0X0009的配置问题。 首先1000Base-T我们使能自动协商。 datasheet中有描述:
All 1000BASE-T PHYs are required to support Auto-Negotiation.
其次就是master 和slave的选择,在自动协商的第二个要素Auto-Negotiation of Master or Slave Resolution中,其中8.4.3.2部分的介绍是这样的:
If 1000BASE-T mode is selected during the priority resolution, the second goal of Auto-Negotiation is to resolve Master or Slave configuration. The Master mode priority is given to the device that supports multiport nodes, such as switches and repeaters. Single node devices such as DTE or NIC card takes lower Master mode priority.
也就是说我们需要将switch配置为master,把PHY配置为slave。通过寄存器0X0009进行配置,看是否能解决您的问题?
您好,我们把phy配为slave模式也还是同样的情况,把phy配成sgmii模式的话,可以固定phy的速率吗,因为mac层的sgmii是千兆的。或者使用phy的sgmii模式还有其他需要配置phy的选项吗?类似是否使能AN这样的配置?
您好,DP83867是支持4线或6线的SGMII mode的。 关于您的这个问题,我这边帮您再看下。
您好,SGMII肯定是enable的,在帖子的寄存器表中,我们地址0x10寄存器的值是0x5848,bit11位为1。而且从switch芯片侧的串口打印能够看到这条链路up上了,但是phy这边一直up不上。
您好,我的switch和PHY 83867接口是SGMII,通过Digital Loopback测试switch->PHY是通的,可以link up检测link status也置1,但是关闭loopback后,一直link不上,初步问题可能出在PHY->RJ45->PC机,想问您一下PHY->RJ45->PC机,需要去操作哪几个寄存器?
您好,我们也是switch-phy-RJ45-PC/商用交换机,您有把phy的三个LED灯接出来吗?这三个灯应该是10M亮一个,100M亮两个,1000M亮三个。我们现在是打开phy的AN功能后,phy的三个灯可以根据接入的速率自行调整,switch侧能看到与phy连接的链路up上了,但是也是不通。我觉得你们可以尝试操作下phy的AN功能寄存器。