This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: 千兆网速率无法实现

Part Number: DP83867IR

DP83867芯片和电脑可以成功实现1000Mbps网速的自协商,但是主控器的无法通过PHY芯片实现网络通信,我们进行了以下测试:

1.主控器通过MAC接口发送固定长度数据至PHY芯片,电脑未能侦听到任何网络数据包

2.电脑发送固定长度数据时,主控器依然无法收到有效数据

3.当手动配置电脑网卡为10/100Mbps的速率时,网络通信时正常的。

4.用示波器观察DP83867芯片的GTX_CLK信号,有明显的的-1.24V的直流偏量。当不接PHY芯片时,主控器输出的GTX_CLK信号直流偏量-0.42V

附件1:DP83867芯片的设计原理图,与主控器MAC的接口都是直连的

附件2:是使用示波器读取的GTX_CLK信号,以及DP83867芯片三路供电电源信号波形图

附件1:DP83867IRPAP原理图.pdf

附件2:示波器波形.docx