HI,我最近在选多个CAN总线应用,查到TCAN1042,我想请教的是,根据数据手册,在STB状态下,每个CANH和CANL内部一个弱的下拉电阻。我想问的是,如20个CAN链接的总线条件下,如果18个处于STB状态,只有2个在STB=0的正常状态,那么根据手册上的说法,此时会有18个电阻将总线下拉到地,而只有2个芯片以很弱的(15K)的电阻将其驱动到2.5V,那这种情况下,18个下拉电阻会将这个2.5V拉到接近地了。。。。此系统这种条件下能正常工作吗。。。。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,我最近在选多个CAN总线应用,查到TCAN1042,我想请教的是,根据数据手册,在STB状态下,每个CANH和CANL内部一个弱的下拉电阻。我想问的是,如20个CAN链接的总线条件下,如果18个处于STB状态,只有2个在STB=0的正常状态,那么根据手册上的说法,此时会有18个电阻将总线下拉到地,而只有2个芯片以很弱的(15K)的电阻将其驱动到2.5V,那这种情况下,18个下拉电阻会将这个2.5V拉到接近地了。。。。此系统这种条件下能正常工作吗。。。。
不对啊,Activate low power Standby mode by setting STB terminal high. In this mode the bus transmitter will not send
data nor will the normal mode receiver accept data as the bus lines are biased to ground minimizing the system
supply current. Only the low power receiver will be actively monitoring the bus for activity. RXD indicates a valid
wake up event after a wake-up pattern (WUP) has been detected on the Bus. The low power receiver is powered
using only the VIO pin. This allows VCC to be removed reducing power consumption further。
你看这个9.4.3描述。他是the bus lines are biased to ground被拉到地了,而且你看你F9.2,描述的STB条件下,内部是拉到地的。。。那跟这个描述有区别啊,而且如果偏置到VCC/2。你手册里面的STB功耗也 不满足啊。。。。
我找到了我印象里的这个电路,如下链接帖子中的回复,但是这个是将信号作为共模信号注入CAN总线的测试电路。
关于上面进入standby模式的节点拉低总线电压的情况,我想应该控制进入standby 节点的比率以控制总线电压。
其实,没有standby模式的收发器也存在泄漏路径的问题,只是相对小一些,因此建议使用带有高阻抗接收器的收发器,以尽量减少增加到总线上的总泄漏。