This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不对啊,Activate low power Standby mode by setting STB terminal high. In this mode the bus transmitter will not send
data nor will the normal mode receiver accept data as the bus lines are biased to ground minimizing the system
supply current. Only the low power receiver will be actively monitoring the bus for activity. RXD indicates a valid
wake up event after a wake-up pattern (WUP) has been detected on the Bus. The low power receiver is powered
using only the VIO pin. This allows VCC to be removed reducing power consumption further。
你看这个9.4.3描述。他是the bus lines are biased to ground被拉到地了,而且你看你F9.2,描述的STB条件下,内部是拉到地的。。。那跟这个描述有区别啊,而且如果偏置到VCC/2。你手册里面的STB功耗也 不满足啊。。。。
我找到了我印象里的这个电路,如下链接帖子中的回复,但是这个是将信号作为共模信号注入CAN总线的测试电路。
关于上面进入standby模式的节点拉低总线电压的情况,我想应该控制进入standby 节点的比率以控制总线电压。
其实,没有standby模式的收发器也存在泄漏路径的问题,只是相对小一些,因此建议使用带有高阻抗接收器的收发器,以尽量减少增加到总线上的总泄漏。