This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB925QSEVB: DS90UB925/DS90UB948使用INTB引脚无法透传中断信号

Part Number: DS90UB925QSEVB


925/948工作在repeater模式下,主机端已经可以获取到触摸屏数据,但是触摸屏的中断信号接在了948的BISTC / INTB_IN,通过lvds传输给925, 925通过INTB引脚接到到主机,但是触摸屏中断信号变化时,INTB引脚量不到信号变化。

这种中断连接方式之前在别的项目中也是这样连接的,但是不清楚怎么配置的,请问如果要透传中断信号,925和948需要怎么配置呢?