Part Number: TUSB8020B
你好,我有个问题想咨询下,我用TUSB8020B做USB3.0 HUB,目前发现下行端口1可以正常识别USB3.0设备,速率是SuperSpeed,端口2只能识别USB2.0,速率是High-speed,原理图如下,请问这个是哪里设置了吗USB.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,USB3.0需要最小900mA的电流,您采用的是自供电还是总线供电方式?
如果总线供电,那么上行端口提供的电流至少要大于1.8A,才能保证两个下行端口每个端口至少900mA的电流。
您好,我看了下TUSB8020的电路,上行端口的TX和RX这里没接错吧,因为我看您将net名字已经改了,不知是否为了和controller的引脚对应改的,再确认下电路。
另外,上电时序是否也满足datasheet中的要求?

您好,我对照demo的电路看了下,SS 差分对上需要加AC耦合电容,demo上使用的是0.1uF,我看port1 也没加, 但是推荐SS 差分对上加上比如0.1uF耦合电容。请参考EVM user's guide Page9的原理图: