This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125DF1610: DS125DF1610

Part Number: DS125DF1610
Other Parts Discussed in Thread: DS125MB203,

Hi Ti,

 DS125DF1610 branch card.pdf

    硬件通道如下:背板 <=> ds125df1610  <=> ds125mb203 <=> 面板10G/1G光模块。

    可以通过i2c通道 ds125df1610ds125mb203,进行配置。


    问题:背板过来的信号,无论是1G信号, 还是10Gxfi信号,面板光口都不link(自环和对接其它设备,都不Link.

    ds125df1610芯片采用上电默认配置,ds125mb203采用的也是默认值,ds125mb203的寄存器如下:

root@ebang:/$i2cdump -f -y 20 59

     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef

00: 08 00 00 00 00 00 10 01 00 00 ff 70 00 00 00 2f    ?.....??...p.../

10: ad 82 00 00 00 00 2f ad 82 00 00 00 00 2f ad 82    ??..../??..../??

20: 00 00 00 00 2f ad 82 00 0c 00 00 00 2f ad 82 00    ..../??.?.../??.

30: 00 00 00 2f ad 82 00 00 00 00 2f ad 82 00 00 00    .../??..../??...

40: 00 2f ad 82 00 00 38 00 05 00 00 00 00 00 00 00    ./??..8.?.......

50: 00 46 00 00 00 00 10 64 21 00 54 54 00 00 00 00    .F....?d!.TT....

60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

root@ebang:/$^C

    

   疑问:

  1. ds125df1610芯片和ds125mb203,有没有透传模式或by-pass模式,因为目前不Link,我无法定位是ds125df1610芯片的问题,还是ds125mb203的问题?
  2. ds125df1610芯片的寄存器很多,对于背板过来的10G xfi信号,需要重点配置哪些寄存器?
  3. 目前ds125df1610芯片采用的是默认上电配置。之前,也手动配置过其它值,也不link
  4. 也试过ds125mb203pin mode,也不link
  5. 麻烦提供一下:DS125DF1610DS125MB2032颗芯片的IBIS模型文件。
  • 1.  这两个器件没有透传功能。

    2. 关于这两个器件的link问题,我这边需要再看下。

    3. 抱歉,这两个器件都没有提供IBIS model,但是可以在其产品主页上申请IBIS -AMI model:

x 出现错误。请重试或与管理员联系。