Part Number: DS125DF1610
Other Parts Discussed in Thread: DS125MB203,
Hi Ti,
硬件通道如下:背板 <=> ds125df1610 <=> ds125mb203 <=> 面板10G/1G光模块。
可以通过i2c通道 ds125df1610和ds125mb203,进行配置。
问题:背板过来的信号,无论是1G信号, 还是10G的xfi信号,面板光口都不link(自环和对接其它设备,都不Link).
ds125df1610芯片采用上电默认配置,ds125mb203采用的也是默认值,ds125mb203的寄存器如下:
root@ebang:/$i2cdump -f -y 20 59
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: 08 00 00 00 00 00 10 01 00 00 ff 70 00 00 00 2f ?.....??...p.../
10: ad 82 00 00 00 00 2f ad 82 00 00 00 00 2f ad 82 ??..../??..../??
20: 00 00 00 00 2f ad 82 00 0c 00 00 00 2f ad 82 00 ..../??.?.../??.
30: 00 00 00 2f ad 82 00 00 00 00 2f ad 82 00 00 00 .../??..../??...
40: 00 2f ad 82 00 00 38 00 05 00 00 00 00 00 00 00 ./??..8.?.......
50: 00 46 00 00 00 00 10 64 21 00 54 54 00 00 00 00 .F....?d!.TT....
60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
root@ebang:/$^C
疑问:
- ds125df1610芯片和ds125mb203,有没有透传模式或by-pass模式,因为目前不Link,我无法定位是ds125df1610芯片的问题,还是ds125mb203的问题?
- ds125df1610芯片的寄存器很多,对于背板过来的10G xfi信号,需要重点配置哪些寄存器?
- 目前ds125df1610芯片采用的是默认上电配置。之前,也手动配置过其它值,也不link。
- 也试过ds125mb203的pin mode,也不link。
- 麻烦提供一下:DS125DF1610和DS125MB203这2颗芯片的IBIS模型文件。