设计中使用TRF3765芯片作为PLL,电路板设计参考TRF3765评估板,基本上和评估板完全一样。设计: SPI配置和读取正确,配置芯片锁定在1GHz时钟上。结果:频谱仪上看1GHz时钟锁定,单在两边每隔2.5MHz都有一个频率,比1GHz幅度小个15dB左右,其中俭相频率设定的就是2.5MHz,锁定指示一直显示为低。现在就是不知如何能消除鉴相频率。请帮助解答,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我把CP电流调低了,之前一直设定最大值,现在杂波小多了。应该和PCB有关。
之前用AD9517,CP比这个还高呢,不过杂波貌似也没这么大。可能TI 的PLL的泵电流普遍小吧。