This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM26LS31: AM26LS31作为外设使用

Part Number: AM26LS31


您好。

我现在使用2.5V的IO输出单端信号到AM26LS31的输入引脚,

但是AM26LS31是5V供电,

它的输入引脚会不会反灌电流把我的输出IO口烧坏呢?

  • 您好,下面是AM26LS31输入电压的阈值电压:Vih(min)=2V,Vil(max)=0.8V。

    如果2.5V IO输出能直接满足AM26LS31的输入的话,需要满足:

    2.5V输出的Voh(min)>2V (AM26LS31的Vih)

    2.5V 输出的Vol(max)<0.8V(AM26LS31的Vil)

    而2.5V CMOS输出的Vohy(min)=2V ,Vol(max)=0.4V 

    所以是可以直接连接的,不需要电平转换器件。