Part Number: AM26LS31
您好。
我现在使用2.5V的IO输出单端信号到AM26LS31的输入引脚,
但是AM26LS31是5V供电,
它的输入引脚会不会反灌电流把我的输出IO口烧坏呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM26LS31
您好。
我现在使用2.5V的IO输出单端信号到AM26LS31的输入引脚,
但是AM26LS31是5V供电,
它的输入引脚会不会反灌电流把我的输出IO口烧坏呢?
您好,下面是AM26LS31输入电压的阈值电压:Vih(min)=2V,Vil(max)=0.8V。

如果2.5V IO输出能直接满足AM26LS31的输入的话,需要满足:
2.5V输出的Voh(min)>2V (AM26LS31的Vih)
2.5V 输出的Vol(max)<0.8V(AM26LS31的Vil)
而2.5V CMOS输出的Vohy(min)=2V ,Vol(max)=0.4V
所以是可以直接连接的,不需要电平转换器件。