This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
Is SN65HVD267D compatible with CAN2.0?
This is because the STM MCU (STM32F722RET7) does not support CAN FD (only CAN 2.0) and our sensors are specifically designed for CAN 2.0, not CAN FD.
Based on the above, can we use the SN65HVD267D as CAN2.0 interface IC?
Thanks.
Kaipo Tu
您好,SN65HVD267D 是物理层的器件,CAN2.0是CAN数据包的格式标准,没有指定是物理层的要求。 那么连接到HVD267的CAN控制器需要支持CAN2.0.
您参考下, 之前也有客户咨询过类似的问题,下面是E2E的工程师给的回复。