Dear Sir,
Is SN65HVD267D compatible with CAN2.0?
This is because the STM MCU (STM32F722RET7) does not support CAN FD (only CAN 2.0) and our sensors are specifically designed for CAN 2.0, not CAN FD.
Based on the above, can we use the SN65HVD267D as CAN2.0 interface IC?
Thanks.
Kaipo Tu