This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD267: Is SN65HVD267D compatible with CAN2.0?

Part Number: SN65HVD267

Dear Sir,

Is SN65HVD267D compatible with CAN2.0?

This is because the STM MCU (STM32F722RET7) does not support CAN FD (only CAN 2.0) and our sensors are specifically designed for CAN 2.0, not CAN FD.

Based on the above, can we use the SN65HVD267D as CAN2.0 interface IC?

Thanks.

Kaipo Tu

x 出现错误。请重试或与管理员联系。