Other Parts Discussed in Thread: DP83620, AM3354, DP83640
在我的设计中,使用了两个光口,采用的设计为TI的AM3354+DP83620+安华高的5803Z。
接口方面,我使用了3354自带的RMII接口,两个PHY各占用一个RMII接口,采用的模式为PHY主模式,时钟设计为25M晶振.
由于考虑到单双路的问题,我们把两个ETH是分开的,但我总觉得这个图哪里不对,在这种应用中,DMIO和MDC是必须的吗?有什么不对的地方请各位批评指正!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢您的回复!
DP83620的TX要上拉这个我可以理解,但是这个阻值有什么依据吗?还有那个C12,C13我不是很清楚这个器件是做什么用的,对该器件本身有没有什么要求?例如误差、温漂、封装等,AFBR5803侧我是参考了该器件的Datasheet,参考附件。
另外MDC和MDIO我一直是百思不得其解,根据资料显示,这两个管脚一个是时钟,一个是数据,它主要是MAC对PHY执行一些读写的命令。再看其他人的DP83640,DP83848的设计,他们都是使用了这两个管教,如果不使用这两个脚,我的PHY的地址MAC怎么去认定呢,还有PHY的寄存器MAC怎么去操作呢?MAC地址又放在哪里呢?
(鉴于本人刚解除ETH设计这一块,可能有些问题比较肤浅,但我不是说什么资料都不看的伸手党,再者边上也没什么人可以请教,英语也不太好,所以请谅解!)
在datasheet的5.5节“PHY ADDRESS” 有描述,pin42---46